No board detected on any of specified UART communication ports.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No board detected on any of specified UART communication ports.

227 Views
Renjie-Wang
Contributor II

Hello.

I am preparing to use the MPC5744 REV E for MBDT development work

  • flashing the rbf file in S32

RenjieWang_0-1726737643043.png

RenjieWang_1-1726737726129.png

RenjieWang_2-1726737751749.png

  • Compiling the gpio_mpc574x.mdl file added the Freemaster Config module

RenjieWang_3-1726737828407.png

 

  • using RAppID_BL.exe to flash the bootloader to the MPC5744 REV E

RenjieWang_5-1726738011358.png

However, when I attempt to connect MPC5744 with Freemaster, I receive the error ‘No board detected on any of the specified UART communication ports

RenjieWang_4-1726737934516.png

Attached are the programs I used 

Thank you for your response

0 Kudos
Reply
0 Replies