NXP Simulink library for MPC5777C and MPC5777E

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Simulink library for MPC5777C and MPC5777E

1,749 Views
TLin3
Contributor III

Hi
When selecting MCU MPC5777C or MPC5777E some blocks show the following error "The selected MCU has no support in MBDT for this peripheral".

https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/NXP-Simulink-library-for-MPC5777C/m-p/1...

People have the same issue before


MBDT for MPC57xx version 3.2.0 is already installed.

Still appear to have some error.

Could you look into this issue, please?

TLin3_0-1679416080981.png

TLin3_1-1679416089341.png

 

 

Thanks

0 Kudos
Reply
3 Replies

1,696 Views
stefancinipeanu
NXP Employee
NXP Employee

Hello, @TLin3 

NXP`s MBD Toolbox for MPC57xx platform reunites 2 major MPC MCU families: MPC574x and MPC577x. As far as I can see in your attached pictures, you are trying to use ADC and PWM peripherals.

Notice that MPC574x family has the ADC and FlexPWM peripherals, while the MPC577x family uses the EQADC peripheral for A/D conversions and eMIOS peripheral for PWM signals generation. You can check out the reference manuals for both MCUs for more information.

stefancinipeanu_0-1679566676146.png

Hope this helps!

Regards,

Stefan.

0 Kudos
Reply

1,734 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I am redirecting your thread to MDBT community.

MDBT team answer only via that community, so you will get most accurate help there.

Best regards,

Peter

0 Kudos
Reply

1,721 Views
TLin3
Contributor III

Hi Peter @petervlna 

Thanks, and hopefully I will get support from NXP team soon.

 

0 Kudos
Reply