MotorGD pre-drive config problems

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MotorGD pre-drive config problems

跳至解决方案
12,151 次查看
haoxue1027
Contributor V

@adriantudor Hello

I have set the config as your advice,

but the GD3000 also did not work.

I found that the J1-1(GD_EN) was always zero.

haoxue1027_0-1599147404813.png

 

Could you test my simulink(test1) and check if the same problems appear?

And I added the GD_EN to the stateflow,but the deadtime was still 15us.

haoxue1027_1-1599147436137.png

Could you help me check the model(test 2) and find the reason ?

best regards

hao

标签 (1)
0 项奖励
回复
1 解答
11,877 次查看
adriantudor
NXP Employee
NXP Employee

@haoxue1027 Hi Hao,

Please see my jumpers setup and if you want to try it (this one it's working with default pins and SPI0). I want to mention that this setup it's working for me but you have to remove 2 resistors from DEVKIT-MOTORGD : R70 and R73. The reason to remove those two resistors is that the output impedance of the level shifter it affect the signal if at the output is connected a pullup or pulldown resistor lower than 50kohm.

Your PWM output it's normal. 

Best regards,

Adrian

MOTORGD.jpg

MPC5744P.jpg

在原帖中查看解决方案

16 回复数
12,143 次查看
adriantudor
NXP Employee
NXP Employee

Hi @haoxue1027  ,

Unfortunately, I don't have Rev. E at this moment, but, I will try to help you.

First thing if you don't use the TPP interrupt, please disable it (uncheck the red box). 

 

TPP int.JPG

Then check jumpers: J28, J22, J31 must be set according to your setup (1-2 for 3.3V or 2-3 for 5V),

J29 - off, J23 - off. And be sure that you power the DEVKIT_MOTORGD using J7 connector placed on MOTORGD.

Please let me know if that helps.

Best regards,

Adrian

0 项奖励
回复
12,072 次查看
Masons
Contributor I

NXP Ultra-Reliable MCUs Development Platforms are a small, cost-effective evaluation, and development system for quick application, prototyping, and demonstration using Ultra-Reliable Automotive and Industrial MCUs.

0 项奖励
回复
12,068 次查看
haoxue1027
Contributor V

really?

At least so far , the pre-drive SPI problem is still unresolved.

0 项奖励
回复
12,133 次查看
haoxue1027
Contributor V

Hello,Adrian

I think your advices "J29 - off, J23 - off“  mean no jumper .

If that ,I always set the jumpers as your recommands.

This time,I did not use the TPP interrupt, and tried again.,but I also didnot work.

In additon, Devkit-MOTORGD also powers base board in my power configration.

It means that the J39(jumper on  1-2 ),J43,44,45(jumper on 2-3).

Does this affect the output?

best regards

hao

0 项奖励
回复
12,111 次查看
adriantudor
NXP Employee
NXP Employee

Hi @haoxue1027 ,

Yes jumper off mean no jumper and routing the power from Devkit-MOTORGD to MPC5744P board it shouldn't affect the output.

I will try to get an MPC5744P Rev. E, in the next days, and I will find the problem.

Best regards,

Adrian

 

0 项奖励
回复
12,108 次查看
haoxue1027
Contributor V

Hello,Adrian

Thank you very much for replying.

I am looking forward to your news.

best regards

hao

0 项奖励
回复
12,088 次查看
adriantudor
NXP Employee
NXP Employee

Hi @haoxue1027 ,

 

After analyzing with an oscilloscope I found that the SPI signals, and CS signal set in the TPP config block, they do not have the right shape (waveform) after the level shifter placed on the MPC board. I'm not sure about the cause but here is what you can do.

First, you must disable the outputs of the level shifter IC connected to SPI input signals of GD3000. By disabling its outputs we can then connect other SPI pins with wire jumpers to the same SPI inputs of GD3000.

So, to disable the outputs of this level shifter IC (U104) (placed on MPC5744P EVB) you must connect jumper J23. Now we must reroute other SPI signals to the same GD3000 inputs. I chose SPI 1 instance with pins: PA6 - SCK, PA7 - SOUT, and PA8 - SIN. Then I connected these pins with wire-jumpers to LT_PC5, LT_PC6, and LT_PC6. By disabling outputs of U104 we have disconnected the CS pin too, so I chose PTA3 to connect to LT_PE15.

I have updated your test1 project with what I told you here.

 

Best regards,

Adrian

0 项奖励
回复
12,039 次查看
haoxue1027
Contributor V

Hello,Adrian

I have connected the jumper 23 and SPI1 pins by wirejumpers.

But it still did not work. I found the LT_PA11 pin was kept zero.

After that I used the stateflow to configure the initialization sequence as the same SPI1 config.

The deadtime was still 15us.

It was so longtime.

Can you help me check it again by test2 as mentioned before?

Thank you very much

best regards

hao

0 项奖励
回复
12,042 次查看
haoxue1027
Contributor V
破坏者

Hello,Adrian

I have connected the jumper 23 and SPI1 pins by wirejumpers.

But it still did not work. I found the LT_PA11 pin was kept zero.

After that I used the stateflow to configure the initialization sequence as the same SPI1 config.

The deadtime was still 15us.

It was so longtime.

Can you help me check it again by test2 as mentioned before?

Thank you very much

best regards

hao

0 项奖励
回复
12,061 次查看
haoxue1027
Contributor V

Hello,Adrian

I have connected the jumper 23 and SPI1 pins by wirejumpers.

But it still did not work. I found the LT_PA11 pin was kept zero.

After that I used the stateflow to configure the initialization sequence as the same SPI1 config.

The deadtime was still 15us.

It was so longtime.

Can you help me check it again by test2 as mentioned before?

Thank you very much

best regards

hao

0 项奖励
回复
12,023 次查看
adriantudor
NXP Employee
NXP Employee

Hi @haoxue1027 ,

 

I checked the "test2" project, and the initialization of GD3000 it fails too, due to SPI level shifter (I think). So I recommend you to used TPP blocks and try to use other SPI instance, not the default one. 

Have you tried a simple example using MBDT to check your setup ?

Is your power source delivering 12V and at least 1A ?

 

Best regards,

Adrian

0 项奖励
回复
12,010 次查看
haoxue1027
Contributor V

@adriantudor Hello,Adrian

Thank you for replying.

I am so sad to hear that test 2 was failed.but it can run in my board.just the deadtime was 15us.

I have try to use the SPI in the TPP blocks as you mentioned,but it still failed.

I have tested the demo of ADC,FLEXPWM, Etimer and so on , it was ok.

So I think the setup is ok. In addition ,the Power source can provide 24V/5A at most.

You have said that the SPI level shifter seemed not goodwork.

Does it means that there is a bug in the hardware or software?

Did you have any other recommends?

Thank you very much.

best regards

hao

0 项奖励
回复
11,924 次查看
adriantudor
NXP Employee
NXP Employee

Hi @haoxue1027,

I hope that you have not connected your power source when it was set to 24V, because in that case, at least one o your boards can have some electronic components burned. The power source should be set to 12V and it's highly recommended to have overcurrent protection enabled and set to 1A at the beginning and after your setup and code is working properly you can increase overcurrent according to your needs.

It's a good thing that you could test a few demos. 

My recommendation for you is to try your "test1" project with your jumper setup (using SPI0) and after the flashing process has been finished, create a power cycle(power off, wait a few seconds then power on both boards). Please let me know if that works for you. 

 

Best regards, 

Adrian

 

 

0 项奖励
回复
11,887 次查看
haoxue1027
Contributor V

@adriantudor Hello,adrian

I found there was a slight error in your proposed PIN connection(the location of PC5,6,7.).

So I have tested again like following. 

haoxue1027_0-1600229795087.png

Fortunately, it worked as deadtime config(1000ns)!~~~A power cycle does not seem neccessary.

But there is a step in the PWM signal like following.

I want to confirm again, Is this normal ?

haoxue1027_1-1600230158142.png

Thank you very much.

best regards

hao

 

 

11,878 次查看
adriantudor
NXP Employee
NXP Employee

@haoxue1027 Hi Hao,

Please see my jumpers setup and if you want to try it (this one it's working with default pins and SPI0). I want to mention that this setup it's working for me but you have to remove 2 resistors from DEVKIT-MOTORGD : R70 and R73. The reason to remove those two resistors is that the output impedance of the level shifter it affect the signal if at the output is connected a pullup or pulldown resistor lower than 50kohm.

Your PWM output it's normal. 

Best regards,

Adrian

MOTORGD.jpg

MPC5744P.jpg

11,849 次查看
haoxue1027
Contributor V

@adriantudor hello,Adrian

I will try to default pin and SPI0 later.

Thank you for helping me to solve this problem.

best regards

hao

0 项奖励
回复