Motor Control Class: Lecture 7 - Commutation Algorithm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Motor Control Class: Lecture 7 - Commutation Algorithm

4,470 Views
dumitru-daniel_
NXP Employee
NXP Employee

In this 7th lecture of the motor control course we discuss about how can we implement the software algorithm for rotating the motor in clockwise or counter clockwise directions. After algorithm implementation we are going to set the model using Software-in-the-Loop (SIL) and Processor-in-the-Loop (PIL) simulation for testing and validation. 

 

Main topics:

    - How the commutation tables are implemented;

    - How to define the requirements for the software algorithm;

    - How to implement the commutation software algorithm;

    - How to use Software-in-the-Loop (SIL) for algorithm testing and validation;

    - How to use Processor-in-the-Loop (PIL) for algorithm testing and validation;

 

Objectives:

    - Understand how commutation loop-up-tables works;

    - Implement from scratch Simulink model for 6-step commutation;

    - Understand how to convert any model to Software-in-the-Loop (SIL) ;

    - Understand how to convert any model to Processor-in-the-Loop (PIL);

 

NOTE: Chinese viewers can watch the video on YOUKU using this link

注意:中国观众可以使用此链接观看YOUKU上的视频

186912_186912.JPG1.JPG186911_186911.JPG2.JPG186913_186913.JPG3.JPG

 

NOTE: Chinese viewers can watch the video on YOUKU using this link

注意:中国观众可以使用此链接观看YOUKU上的视频

186914_186914.JPG4.JPG186915_186915.JPG5.JPG

 

NOTE: Chinese viewers can watch the video on YOUKU using this link

注意:中国观众可以使用此链接观看YOUKU上的视频

186916_186916.JPG6.JPG186917_186917.JPG7.JPG

 

Additional information:

    - pdf attached with slides shown in these videos;

    - Simulink models used in these videos: BLDC commutation, SIL and PIL

 

Original Attachment has been moved to: Lecture7.zip

Update revisions:

February 25, 2019

May 06, 2020

0 Replies