EV Powertrain source: carmagazine.co.uk |
INTRODUCTION
Nowadays, are we witnessing the start of a global revolution within the automotive industry, where more and more car manufacturers are trying to compete in the rising sector of electrical vehicles. At the core of this revolution sits the "work horse" of modern transportation: the humble electric motor.
In this module of the 3-Phase PMSM Control Workshop with NXP's Model-Based Design Toolbox , we are going to discuss about the FOC for traction motors and how to control the torque produced by PMSM. The control method is generic and may be applicable to all sort of means of transportation: trains, buses, bikes, scooters and modern day cars.
In a car with internal combustion engine each time you press the gas pedal, the throttle valves open, more fuel and air is injected into cylinders resulting in a stronger explosion that sends the piston down with a stronger force. This linear force pointed downward is converted via the crankshaft into a rotational movement with a certain amount of torque given by the product between the force and rod length. Therefore, each time you press the "pedal to the metal" you control an amount of torque the engine is capable of. Under normal driving conditions the speed of the vehicle is regulated in driver's head that ultimately decides to push the acceleration pedal more or less.
The purpose of this article is to replicate such control system. The user will be able to set a torque reference and the motor will obey that command speeding up or slowing down based on how much torque is being demanded. In this module we are going to learn how to:
In Fig. 1, which represent the global application mapping diagram as discussed in Module 3: System Partitioning , are shown the new hardware blocks that are going to be configured and used to perform the PMSM FOC Torque Control highlighted in green relative to the ones already configured so far in the previous modules of this workshop. We are going to reuse and enhance the model developed in Module 6: Current Sensing (Part 1/2) and Module 6: Current Sensing (Part 2/2) which will allow us to test the application in real time on S32K144 3-phase PMSM Development Kit|NXP . The interactions between host PC and hardware will be done via OpenSDA serial communication that will be used to download the code generated from MATLAB and to visualize various control signals with FreeMASTER. In addition, the user can start and control the motor speed from the SW2 and SW3 push button present on the S32K144 Evaluation Board|NXP . A three color LED will be used to signal the control states and faults.
Fig. 1: Application Mapping - new HW & SW modules used for FOC Torque Control are highlighted in green |
TORQUE CONTROL
The Torque Control replicates the behavior of internal combustion engine. As is was explained in Module 2: PMSM and FOC Theory to achieve the adequate motor response we need to:
In Fig. 2, is shown the block diagram of the Torque Control system proposed for implementation. The Field Oriented Control is executed in the FAST CONTROL LOOP block that is executed based on a ADC trigger at each 100 microseconds. This subsystem receives the references values for currents in Q (torque) and D (flux) axis and the currents measured from the ADC and outputs the PWM duty cycles commands that controls the 3-phase inverter.
The toque and flux references are computed in the SLOW CONTROL LOOP block that is triggered at each 1 milisecond based on the same ADC events as the FAST CONTROL LOOP. The speed and torque commands are received via the UART or from on board push buttons and transformed based on a LUT into actual torque and electric angle increments.
Fig. 2: FOC Torque Control - Block Diagram |
As you can see in Fig. 2, we have only one loop that is closed: current loop. The outer speed loop is still open, hence it does not prevent us for implementing the torque control even if this is not ideal. The outer speed loop will be closed in the next module of this workshop.
SLOW CONTROL LOOP
The block diagram of the functions implemented on SLOW CONTROL LOOP is shown in Fig. 3. At each startup, a special alignment sequence is executed in order to move the PMSM rotor into a particular well known position - rotor magnetic D axis is align with PMSM stator phase A. The rotor alignment is a key aspect in torque control since we want to produce the highest torque available and that can only be done if we maintain a 90 electrical degrees between Q axis and rotor magnetic flux axis D
Fig. 3: Slow Control Loop - Block diagram for Torque Control |
The alignment is achieved by injecting a current into the D-axis, forcing this way the rotor magnets to align with the magnetic field produced in the stator. For the rotor alignment we need two parameters:
Once the rotor alignment is completed the speed command is transformed into the torque command via a LUT similar with the method from Module 5: V/F Scalar Control
In the same time with torque reference computation, the actual electric angle increment is computed in order to rotate the motor.
FAST CONTROL LOOP
The block diagram of the functions implemented on FAST CONTROL LOOP is shown in Fig. 4. As it can be noticed this is the complete diagram of the Field Oriented Control as discussed in Module 3: System Partitioning
Fig. 4: Fast Control Loop - Block diagram for Torque Control |
Based on the reference input values of Torque (Iq), Flux (Id) and the PMSM measured phased currents, after PARK forward transformation the appropriate control voltages for (dq) reference system are computed with the help of two independent PI current controllers. Once the command voltages are obtained, the inverse PARK and CLARKE transformations are used to compute the PWM duty factors via the Space Vector Modulation technique to control the 3-phase inverter MOSFETs.
The theory behind the PI controllers was discussed in Motor Control Class: Lecture 11 - Closed Loop Control
In case of motor electric transfer function the procedure of computing the current controller Kp and Ki gains is the same as the one presented for the speed controller with the observation that Inertia (J) is replaced with Inductance (L) and Friction coefficient (b) is replaced with Resistance (R). The rest of the computations remains similar.
Note, how in the Fig. 4, we are demanding the rotor to move in a desired position based on the computation of the electrical angle (theta) that is derived from the speed reference computed in SLOW CONTROL LOOP. Since there is no loading torque on the motor, we are going to use for demonstration this method of controlling the motor torque in open loop since it is safe and will produce good results. In case there is a loading torque and the rotor alignment is not correct the motor might lose the synchronism and will stall. For such cases you will need:
The Simulink model used to implement all these functionalities is shown in Fig. 5:
Fig. 5: Simulink model for PMSM FOC Torque Control |
Video training: How To Implement and Test Torque Control System for PMSM Using S32K144EVB | ||
---|---|---|
Please watch this video before going further. The rest of the article is a summary of the video.
TORQUE CONTROL SIMULINK MODEL
In this section we are going thru the high level details regarding the implementation of Toque Control model shown in Fig. 5. The model is available for download at the end of the article. In the figures below we are going to discuss only new functionalities added or changed compared to the model implemented in Module 6: Current Sensing (Part 1/2)
ADC Interrupts
Since we need the FOC software routines (SLOW CONTROL LOOP & FAST CONTROL LOOP) to be synchronized with the ADC measurements as it was shown in Fig. 9 from Module 6: Current Sensing (Part 1/2) we are going to modify the PDB1_IRQ to trigger a function call based on ADC conversion complete (COCO) interrupt that corresponds to the AD15 - PMSM Phase B current. For this we are going to use the ADC_ISR block that allows us to read the conversion results and trigger an interrupt in the same time.
Fig. 6: ADC Interrupt trigger for SLOW and FAST Control Loops |
Interrupt Dispatcher
Because the ADC interrupts are synchronized with the PWM frequency, it means that we will get an interrupt at each 100 micro-seconds for a 10kHz switching frequency. That is OK for the FAST CONTROL LOOP which we want to be triggered at each 100 micro-seconds, but for the SLOW CONTROL LOOP that must be scheduled at each 1 mili-seconds we need to implement a sort of dispatching mechanism. This is done in the IRQ_Dispatcher subsystem as shown in Fig. 7.
Fig. 7: Dispatching interrupts to FAST and SLOW CONTROL LOOPS based on ADC HW COCO interrupt |
This block implements a two stage logic:
The dispatching mechanism that keeps a relative execution rate of 10:1 is implemented as:
Fig. 8: Interrupt dispatcher implementation for execution rate 10:1 between FAST vs. SLOW loops |
Slow Control Loop
This subsystem was modified as shown in Fig. 9, to allow:
As Fig. 9 shows, we have kept the same mechanism used for Module 5: V/F Scalar Control to generate the electrical angle profile and the the references for the (dq) system commands.
Fig. 9: SLOW CONTROL LOOP implementation |
Fast Control Loop
This subsystem was enhanced with two PI controllers for each of (dq) axis and the forward PARK and CLARKE transformations that are now used to compute the currents in (dq) reference system starting from the values measured from ADC.
As can be noticed, during the alignment process the PI controllers are bypassed while the commands from SLOW CONTROL LOOP are directly applied as voltage commands to the FOC transformations. This ensure a faster and stronger response, forcing the rotor to align more precisely into the correct positions without additional delays cause by the PI controllers.
Fig. 10: FAST CONTROL LOOP implementation |
Board Controls
The subsystem shown in Fig. 11, implements the logic of reading the push buttons from the S32K144 Evaluation Board|NXP that allows us to change the motor speed manually and the mechanism of LED notification. The LED logic is implemented as:
Fig. 11: I/O board controls |
Protections
The motor and drive protections are implemented in the ADC interrupt routine immediately after the measurements in order to make sure that any fault is addressed as soon as possible. Currently there are three protections implemented but in next modules, additional ones will be added:
If one of these conditions occurs the application will disable the PWM generation immediately and the application will not be able to be resumed until a RESET is issued by the user.
Fig. 12: Protections |
EXPERIMENTAL RESULTS
Using the FreeMASTER attached project we can check the system responses and tune the controllers to responds however we wish on the fly in real time. For demonstration purposes the controller are de-tuned in order to increase the respond time and have easy to understand pictures.
Fig. 13, shows the system response during the alignment sequence, startup and normal operation. You can see that the alignment sequence is lasting for 3 seconds. In this time interval ~1.1 amps are injected in the flux axis in order to force the motor alignment with stator phase A. The correspondence between the (dq) currents and the actual (abc) currents can be clearly observed in Fig. 14.
Fig. 13: Startup sequence: alignment, startup and normal operation showing: - Torque reference (IQ_REF - red) and Actual Torque (IQ - orange) - Flux reference (ID_REF - blue) and Actual Flux (ID - cyan) |
Fig. 14: Startup sequence: alignment, rump-up and normal operation comparison between the (dq) reference system and (abc) reference system - Actual Torque (IQ - orange) and Flux Flux (ID - cyan) in the upper part - Actual PMSM phase current Ia, Ib, Ic |
Fig. 15, shows the PI controllers responses during startup and normal operation. As you can see in order to maintain almost 1.5 amps thru the motor we need only a small amount of control voltage (0.5 volts - on the right axis).
Fig. 15: PI Current Controller behavior: inputs vs outputs - Torque axis response (upper) - Flux axis response (lower) |
Fig. 15, shows that there is plenty of room to play of current controller tuning parameters and improve the system response since the voltage reserve is not reached.
How would you tune the current controllers ? Do you prefer a sharp or a mild response and why is that ?
Update revisions:
March 19, 2018
Update January 28th 2019 - This Simulink model is now available on MATLAB 2018b and MBDT for S32K14x 2018.R1 release
Before using the new models make sure you apply all the hot-patches from here: HotFix: MBD Toolbox 2018.R1 for S32K
Update revisions:
March 18, 2019
May 06, 2020
Hi Leon,
Both values for torque vs flux are chosen based on experiments.
- for the Speed2Torque - you need to choose a starting current that allows the motor to rotate - usually this is the current needed for overcoming the friction or static load. Then you can increase that current linear until the nominal speed is reached.
Probably you have noticed that this FOC Torque Control example is a little bit special. In general if you have a motor without load you can't keep a certain current in Q axis because similar with the DC motors that are powered up with constant voltage, the motor will accelerated until U = E + R*I. To avoid that from happening, the angle used for PARK transformations is set from Speed Profile ramp block. This way i can control the motor torque without having the motor spining like crazy.
- for the D-axis flux, again by experiments i found the appropriate voltage % value (it is a percent of Vdc/2) that is needed to align the rotor magnetic flux of PM with the Stator Phase A magnetic axis. If the value is too small, and the motor cogging torque is high then the rotor might not align properly. You should try the value for the voltage with the rotor aligned in different positions. Based on you motor number of pole pairs you should be able to align the rotor with the same points - over and over again - starting from different positions.
Alternatively you can think in terms of current - usually the alignment current should be closed to the nominal motor current or in some situation if you keep it for a few seconds it might even go higher like 1.5In
Hello dumitru-daniel.popa
for the beginning I have 2 questions for the Slow Loop:
1) How did you calculated the Speed2Torque LUT ? My Motor is without any load at the Moment, did you have applied any load to your Motor ?
2) The required d-axis voltage for alignment is experimental ?