Model Based Design Toolbox for S32K14x Automotive MCU rev2.0 Free cost?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Model Based Design Toolbox for S32K14x Automotive MCU rev2.0 Free cost?

1,490 Views
hayaoki7
Contributor IV
0 Kudos
Reply
2 Replies

1,055 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi hayaoki7‌,

Indeed, all the Model-Based Design Toolboxes from NXP are now cost free. You can use it for free with no fee charge.

The entire suite & ecosystem (IDE for debugging, GCC toolchain, bootloaders) is provided for free - all you need to do is to have an NXP account to download the licences - also free of charge.

You need to have a Matlab environment with Embedded Coder toolbox in order to be able to generate the C code automatically. That is a cost you have to consider but from our point of view we assume you have already such environment.

Hope this helps!

Daniel

0 Kudos
Reply

1,055 Views
hayaoki7
Contributor IV

How Nice

Thank you

0 Kudos
Reply