Many analog signal readings from the same EQADC module on the MPC5777C?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Many analog signal readings from the same EQADC module on the MPC5777C?

934 次查看
ranulf
Contributor IV

It would be helpful to see examples ADC readings made of 3 or more analog signals, preferably from the same EQADC module (either 0 or 1). Apparently the EQADC blocks have the ability to read from more than 2 analog signals, but neither the examples nor the documentation show how to do this. Both of the examples cover cases where only 2 analog signals are read.

How many analog signals can be read by each EQADC module and how many analog signals can be read by the two modules together? It would also be nice to see examples that demonstrate reading a large number of analog channels involving both modules.

0 项奖励
回复
1 回复

901 次查看
ranulf
Contributor IV

The MPC5777C is already supported. See Model-Based Design Toolbox for MPC57xx version 3.2.0

0 项奖励
回复