MPC57xx MBDtoolbox not appears in Simulink Library Browser

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC57xx MBDtoolbox not appears in Simulink Library Browser

跳至解决方案
10,621 次查看
Bing
Contributor II

I followed the quick start guide step by step, everything seems OK during the installation. I'm using Matlab R2021a.

But finally the MPC57xx MBDtoolbox does not appear in Simulink Library Browser. However I can run  MPC57xx MBD examples successfully on devkit.

For a simple comparison, MBDtoolbox for IMXRT does not have the same problem.

Thanks for help.

1 解答
10,558 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @Bing ,

The second option I was telling you about is the "Generate repositories in memory" as show below, when you press the F5 button.

mariuslucianand_0-1627628778962.png

Once I did that, I can see both libraries in my Simulink Library Browser.

mariuslucianand_1-1627628830207.png

Hope this helps,

Marius

 

 

在原帖中查看解决方案

4 回复数
10,608 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @Bing,

Please open the Simulink Library and press the F5 button. Then select the second option and see if the MPC57xx Toolbox appears.

 

Hope this helps,

Marius

0 项奖励
回复
10,598 次查看
Bing
Contributor II

Hi Marius,

I've tried refreshing Simulink Library Browser, but I'm not quite clear with “select the second option” and can not find the entry.

Thanks for helping,

Bing

0 项奖励
回复
10,559 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @Bing ,

The second option I was telling you about is the "Generate repositories in memory" as show below, when you press the F5 button.

mariuslucianand_0-1627628778962.png

Once I did that, I can see both libraries in my Simulink Library Browser.

mariuslucianand_1-1627628830207.png

Hope this helps,

Marius

 

 

10,550 次查看
Bing
Contributor II

Hi @mariuslucianand 

It works! Great help!

MPCtlbx.png

Thanks for guiding,

Bing