MPC57xx MBDtoolbox not appears in Simulink Library Browser

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC57xx MBDtoolbox not appears in Simulink Library Browser

Jump to solution
10,666 Views
Bing
Contributor II

I followed the quick start guide step by step, everything seems OK during the installation. I'm using Matlab R2021a.

But finally the MPC57xx MBDtoolbox does not appear in Simulink Library Browser. However I can run  MPC57xx MBD examples successfully on devkit.

For a simple comparison, MBDtoolbox for IMXRT does not have the same problem.

Thanks for help.

1 Solution
10,603 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @Bing ,

The second option I was telling you about is the "Generate repositories in memory" as show below, when you press the F5 button.

mariuslucianand_0-1627628778962.png

Once I did that, I can see both libraries in my Simulink Library Browser.

mariuslucianand_1-1627628830207.png

Hope this helps,

Marius

 

 

View solution in original post

4 Replies
10,653 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @Bing,

Please open the Simulink Library and press the F5 button. Then select the second option and see if the MPC57xx Toolbox appears.

 

Hope this helps,

Marius

0 Kudos
Reply
10,643 Views
Bing
Contributor II

Hi Marius,

I've tried refreshing Simulink Library Browser, but I'm not quite clear with “select the second option” and can not find the entry.

Thanks for helping,

Bing

0 Kudos
Reply
10,604 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @Bing ,

The second option I was telling you about is the "Generate repositories in memory" as show below, when you press the F5 button.

mariuslucianand_0-1627628778962.png

Once I did that, I can see both libraries in my Simulink Library Browser.

mariuslucianand_1-1627628830207.png

Hope this helps,

Marius

 

 

10,595 Views
Bing
Contributor II

Hi @mariuslucianand 

It works! Great help!

MPCtlbx.png

Thanks for guiding,

Bing