MPC5744p工具箱建模编译出错

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744p工具箱建模编译出错

2,743 Views
q380742432
Contributor I

我用MBD toolbox for 5744p 创建了一个模型,编译的时候提示如下错误,安装了license文件 

0 Kudos
9 Replies

1,960 Views
xielinda
Contributor I

Ni hao!

   Can you tell me where can I download the TSP for 5744?

Hope it helps!

Linda

0 Kudos

1,961 Views
dumitru-daniel_
NXP Employee
NXP Employee

Hi Linda, 

What is TSP ?

Are you referring to Matlab Toolbox for MPC5744 ? That can be downloaded from: https://community.nxp.com/docs/DOC-333913 

Best regards,

Daniel

0 Kudos

1,961 Views
xielinda
Contributor I

HI Daniel

This is message 企业微信截图_15226310969730.png

0 Kudos

1,961 Views
xielinda
Contributor I

HI Daniet.

First Thinks for you give me the link.

yeah that's my want but I can download it well!

Best regards.

Linda

0 Kudos

1,961 Views
dumitru-daniel_
NXP Employee
NXP Employee

Ni hao, 

Do you have a license file generated from the NXP website ?

In case you don't have one, please check this video starting with minute 3.00 about how to install and generate a license file: Motor Control Class: Lecture 1 - Introduction 

Also, can you copy paste the massage you are getting in Chinese before "lic_err"

We have this table with the common license errors: maybe you want to check it out

https://community.nxp.com/thread/449904#comment-908767 

Hope it helps!

Daniel

0 Kudos

1,961 Views
q380742432
Contributor I

hi,Daniel

   when I run the command "mbd_pnt_hostid"   MATLAB will remind me of this error "The index is out of the matrix dimension.
Error mbd_pnt_hostid"  so,i used the second ways to obtain。“ lmhostid -vsn

0 Kudos

1,961 Views
dumitru-daniel_
NXP Employee
NXP Employee

Hello, 

Please check this thread: https://community.nxp.com/thread/453708 I think is the same problem with the same solution applicable

0 Kudos

1,961 Views
q380742432
Contributor I

thanks

0 Kudos

1,961 Views
q380742432
Contributor I

hi,Daniel

I have installed the license file,but it didn't work。Still remind me of this error. Undefined function or variable:lic_err

0 Kudos