MPC5744P for UART and I2C Interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5744P for UART and I2C Interface

跳至解决方案
2,232 次查看
toddchou
Contributor I

Dear Sir 

I am Todd and use MPC5744 for a project . In datasheet , this MCU can program UART interface that using FlexLIN port . However , it did not write some I2C interface . I am not sure , can we program I2C interface that same using FlexLIN , FlexRay or which one can support I2C interface ? 

Looking forward for your feedback. 

Thank you and have a good day.

Todd

0 项奖励
回复
1 解答
2,000 次查看
constantinrazva
NXP Employee
NXP Employee

Hello toddchou@ycsynergy.com.tw‌,

MPC5744P does not have any I2C hardware unfortunately; I'm not sure if you are developing a project using our Simulink toolbox, but if you do you will not find support for I2C as there are no hardware instances available. If you need to have I2C, you can use the SDK for MPC5744P - there you have software support for I2C, this meaning bit-banging of the protocol done by the CPU.

Hope this helps,

Razvan.

在原帖中查看解决方案

2 回复数
2,001 次查看
constantinrazva
NXP Employee
NXP Employee

Hello toddchou@ycsynergy.com.tw‌,

MPC5744P does not have any I2C hardware unfortunately; I'm not sure if you are developing a project using our Simulink toolbox, but if you do you will not find support for I2C as there are no hardware instances available. If you need to have I2C, you can use the SDK for MPC5744P - there you have software support for I2C, this meaning bit-banging of the protocol done by the CPU.

Hope this helps,

Razvan.

2,000 次查看
toddchou
Contributor I

Hello Razvan 

Thanks for your explanation. 

Have a good day 

Todd

0 项奖励
回复