MPC564xL Motor Control Toolbox patch for Matlab/Simulink 2017b

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC564xL Motor Control Toolbox patch for Matlab/Simulink 2017b

2,838 Views
mcgillformulael
Contributor I

Hello,

We are having trouble with the hardware implementation of our MPC564xL with Matlab & Simulink R2017b. Indeed, our Motor Control Toolbox Hardware Implementation blocks are not compatible with R2017b, and return errors when trying to generate code with Simulink. See picture attached. As seen, even the simplest model leads to an error when trying to generate code. "Undefined function 'slsfnagctlr' for input arguments of type 'char'." 

Therefore, I wanted to know if this is an issue that can be fixed? I have seen the same issue on the Community Forum but with a different Microprocessor. Would it be possible to fix the issue also on the MPC564xl?

Kind Regards,

Michael

McGill Formula Electric

Tags (3)
0 Kudos
Reply
2 Replies

2,398 Views
paulvlase
NXP Employee
NXP Employee

Hi mcgillformulaelectric‌,

I've created HotFix_1 for this. Can you please try it and confirm that it works for you?

Thank you,

Paul

0 Kudos
Reply

2,398 Views
mcgillformulael
Contributor I

Hi paulvlase‌,

Thank you for your excellent support. The patch did work!

Best,

Michael

0 Kudos
Reply