MCAN_Receive mode error on RDVCU5775EVM development board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCAN_Receive mode error on RDVCU5775EVM development board

3,450件の閲覧回数
peaces
Contributor III

Hello to everyone
I want to use MCAN_Receive block in "Blocking" mode on the RDVCU5775EVM development board, but I get the error in the picture.
Can you help with this?

0 件の賞賛
返信
4 返答(返信)

3,414件の閲覧回数
peaces
Contributor III

do you have any results?

0 件の賞賛
返信

3,429件の閲覧回数
peaces
Contributor III

Hello @mariuslucianand 

I have reviewed the page before and asked this question because I did not get any results.

 

0 件の賞賛
返信

3,434件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @peaces ,

Can you please have a look at this page?

https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Build-Fails-When-Target-MCU-gt-Family-i...

Hope this helps,

Marius

0 件の賞賛
返信

3,242件の閲覧回数
ahmetsaglam
Contributor I

HI @mariuslucianand 

When we use the MCAN receive block, we encounter the error in the picture.

''''''Error: Simulink Coder Error: The specified port index 'Number' of <S2>/MCAN_Receive should be a number between 0 and 3.'''''

We applied the fields on this page

https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Build-Fails-When-Target-MCU-gt-Family-i...

ahmetsaglam_0-1636530077375.pngahmetsaglam_2-1636530378339.png

 

ahmetsaglam_1-1636530223008.png

Regards 

Ahmet 

0 件の賞賛
返信