MBDToolbox_S32K3xx_1.0.0 License问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBDToolbox_S32K3xx_1.0.0 License问题

924 Views
pt77
Contributor I

运行里面的例子(s32k3xx_can_receive.mdl),会出现如下错误,该如何处理:

License Error: -5, Model-Based Design Toolbox License Invalid, please go to The Model-Based Design Development Toolbox Web Site and include error number.

0 Kudos
2 Replies

761 Views
BillDuley
Contributor III

The link to MBDT S32K31.1.0 does not appear to be functional. Is this purposeful on NXP's part?

https://nxp.flexnetoperations.com/control/frse/download?element=12920897

0 Kudos

886 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hi @pt77 ,

I have attached a link to a thread that addresses this issue (https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K34-build-error/m-p/1371545). Please check the posts here and follow the described steps which could help you with the setup of the toolbox.

Also, please note that the MBDT version you are using is not the latest one. So in case you would like to upgrade to the newest release, please download MBDT for S32K3 v1.1.0.

Hope this helps,

Irina

0 Kudos