MBDToolbox_S32K3xx_1.0.0 License问题

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBDToolbox_S32K3xx_1.0.0 License问题

923件の閲覧回数
pt77
Contributor I

运行里面的例子(s32k3xx_can_receive.mdl),会出现如下错误,该如何处理:

License Error: -5, Model-Based Design Toolbox License Invalid, please go to The Model-Based Design Development Toolbox Web Site and include error number.

タグ(1)
0 件の賞賛
2 返答(返信)

760件の閲覧回数
BillDuley
Contributor III

The link to MBDT S32K31.1.0 does not appear to be functional. Is this purposeful on NXP's part?

https://nxp.flexnetoperations.com/control/frse/download?element=12920897

0 件の賞賛

885件の閲覧回数
Irina_Costachescu
NXP Employee
NXP Employee

Hi @pt77 ,

I have attached a link to a thread that addresses this issue (https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K34-build-error/m-p/1371545). Please check the posts here and follow the described steps which could help you with the setup of the toolbox.

Also, please note that the MBDT version you are using is not the latest one. So in case you would like to upgrade to the newest release, please download MBDT for S32K3 v1.1.0.

Hope this helps,

Irina

0 件の賞賛