MBDT for i.MX RT 105x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBDT for i.MX RT 105x

Jump to solution
1,531 Views
gianpiero_lenta
Contributor I

Is the MBDT supported by the RT105x microprocessor?
From the document "NXP Model-Based Design Toolbox (MBDT) Fact Sheet" it would appear that the micro 105x is not supported.
Who can answer me?

What I don't quite understand is this:
the 106x and 105x share cores, peripheral architecture, and differ only in the amount of internal RAM. Correct? Then why is MBDT not supported?

Thank you

0 Kudos
Reply
1 Solution
1,502 Views
stefancinipeanu
NXP Employee
NXP Employee

Hello @gianpiero_lenta 

Currently, the NXP`s MBD Toolbox for IMXRT1xxx platform does not support IMXRT105x and we do not have any plans to add it in the near future, but we are going to analyze this option.

Regards,

Stefan.

View solution in original post

0 Kudos
Reply
1 Reply
1,503 Views
stefancinipeanu
NXP Employee
NXP Employee

Hello @gianpiero_lenta 

Currently, the NXP`s MBD Toolbox for IMXRT1xxx platform does not support IMXRT105x and we do not have any plans to add it in the near future, but we are going to analyze this option.

Regards,

Stefan.

0 Kudos
Reply