MBDT S32K3xx hardware board missing in Simulink model settings

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MBDT S32K3xx hardware board missing in Simulink model settings

跳至解决方案
2,464 次查看
jpb_cid
Contributor I

I have succesfully installed the 1.2.0 version of the MBDT for S32K3xx microcontrollers + the hardware support packages from the matlab add-ons.

I have access to the library in Simulink, but the hardware board from NXP (NXP S32K3) is missing in the list (attached image).

What can I do to resolve this issue?

Many thanks.

0 项奖励
回复
1 解答
2,456 次查看
dragostoma
NXP Employee
NXP Employee

Hi, @jpb_cid ,

 

Thank you for using our MBDT S32K3 Toolbox. A quick solution to your problem is to close all the Simulink models, then remove the toolbox from the path by running in Matlab command line the following script mbd_s32k3_path('remove'). To re-add the toolbox to the path use the following command mbd_s32k3_path. To run this script, you have to be in the Toolbox root folder, as in the screenshot below. You could also try restarting the Matlab after this.

 

dragostoma_2-1669223536279.png

 

Let me know if any of these suggestions helped you. 

 

Best regards,

Dragos

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,425 次查看
jpb_cid
Contributor I

Hi @dragostoma,

Thank you for coming up with the solution. It was just that we were missing the "Embedded Coder Support Package for ARM Cortex-M Processors" from Mathworks, which was required when executing the mbd_s32k3_path command.

Many thanks and best regards,

Jon.

 

0 项奖励
回复
2,457 次查看
dragostoma
NXP Employee
NXP Employee

Hi, @jpb_cid ,

 

Thank you for using our MBDT S32K3 Toolbox. A quick solution to your problem is to close all the Simulink models, then remove the toolbox from the path by running in Matlab command line the following script mbd_s32k3_path('remove'). To re-add the toolbox to the path use the following command mbd_s32k3_path. To run this script, you have to be in the Toolbox root folder, as in the screenshot below. You could also try restarting the Matlab after this.

 

dragostoma_2-1669223536279.png

 

Let me know if any of these suggestions helped you. 

 

Best regards,

Dragos

0 项奖励
回复