MBDT Related questions on S32K3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MBDT Related questions on S32K3

568 次查看
iverson3ya
Contributor III

1. Can I build my own model for clients to use in MATLAB by S32DS?

2. In the MBDT, I didn't see interfaces related to RMII, SGMII networks, or LIN, RS232/485. So, does this mean only ADC, PWM, MCL, CAN, SPI, UART, GPT, and DIO are available?

0 项奖励
回复
1 回复

549 次查看
iverson3ya
Contributor III

Firstly, I have completed a project using S32DS. Currently,

the client wants to conduct secondary development using MATLAB. My idea is to develop the project in MATLAB through the MBDT, then package it and hide certain modules.

The client could use these modules to control the system, only needing to handle simple applications, such as retrieving data from the CAN or LAN buffer or controlling DIO.

My project includes FreeRTOS and requires modules like LwIP, CAN, FS26, etc.

Would this approach be feasible?

Thank you very much.

0 项奖励
回复