MBDT LIN compile error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MBDT LIN compile error

1,255 次查看
andyknitt
Contributor II

I'm running into some unexpected errors when trying to use the MBDT LIN blocks with the S32K142. 

The LIN master example compile without issue but when I try to use the LIN blocks into my own model I'm getting errors that both LIN_XCVR_ENABLE_GPIO_PORT and LIN_XCVR_ENABLE_MASK are undefined:

error: 'LIN_XCVR_ENABLE_GPIO_PORT' undeclared (first use in this function) PINS_DRV_SetPinsDirection(LIN_XCVR_ENABLE_GPIO_PORT, LIN_XCVR_ENABLE_MASK);

 

When I look at the C code that gets generated from the lin_master_s32k14x.slx example I see these #defines:

34	#define LIN_XCVR_ENABLE_PIN            (9UL)
35	#define LIN_XCVR_ENABLE_MASK           (0x1u << LIN_XCVR_ENABLE_PIN)
36	#define LIN_XCVR_ENABLE_GPIO_PORT      (PTE)

These same #define statements are not present in the C code that gets generated from my model that's using the same LIN blocks.  

A couple questions:

  1. What in the Simulink model for the example project is generating these #define statements?  There is nothing in the GUI for any of the blocks to specify a GPIO pin to use for LIN Transceiver Enable. 
  2. My hardware does not need a LIN Transceiver Enable pin.  How can I get the code to compile without attempting to initialize a GPIO pin for this function?  Again, there is nothing in the Simulink blocks related to this at all (just the TX and RX pins, as I would expect).  

Thanks,

Andy

0 项奖励
回复
2 回复数

1,234 次查看
andyknitt
Contributor II

I was able to work around the compiler error by adding the missing #defines into the Custom Code section of the Simulink model configuration.  

This is a bit of a hack though, and I'd still like to understand the answers to the two questions in the post above.  

andyknitt_0-1676648708170.png

I'm now experiencing a different issue.

When acting as a LIN master, I can successfully send messages to and receive data from slaves if the slaves are all connected and working properly.  However, if I send a message header to get data from a slave that isn't present and the slave doesn't respond, the LIN_ReceiveFrameData seems to be blocking and doesn't allow transmission of any additional headers via the LIN_Master_Send_Header block if it never receives any frame data from the slave.  Is there a way to address this?  I don't see any timeout values in any of the LIN blocks, nor do I see a timeout in the LIN events that can be generated by the LIN_ISR block.  

Any advice would be appreciated.

 

0 项奖励
回复

1,209 次查看
andyknitt
Contributor II

I think I've figured out what's causing the "blocking" behavior if a Slave never sends the data that the Master S32K1xxx is expecting.

The LIN receive Simulink block calls the LIN_LPUART_DRV_RecvFrmData() function, which is technically non-blocking (LIN_LPUART_DRV_RecvFrmDataBlocking() is the blocking version), but it does set the linCurrentState->isBusBusy flag to true, which effectively prevents the other LIN blocks from using the bus. 

andyknitt_0-1676937643827.png

The LIN_LPUART_DRV_MasterSendHeader() function called by the LIN_Master_Send_Header block checks to see if the linCurrentState->isBusBusy flag is true and if it is, returns without sending the header.  

andyknitt_1-1676937656014.png

If the Master never completes receiving data from the Slave (slave goes offline, etc.), the linCurrentState->isBusBusy flag never gets reset and the Master can't send any more headers.   

Allowing a bad slave to prevent further action by the Master is probably not a great idea.  

I modified the lin_lpuart_driver.c file as shown below as a hacky workaround, but modifying the NXP driver source code files is not an ideal long-term solution.  

andyknitt_2-1676937818607.png

A better solution may be to add some checks of the linUserConfig->nodeFunction (MASTER/SLAVE) flag in various places where it makes sense for a Master to do things regardless of slave behavior, but I haven't fully thought through where all of those checks would need to be.  

I'd appreciate any insight into other possible solutions or more "correct" workarounds for this issue.  

0 项奖励
回复