I am using Ubuntu machine for the development
I successfully set up S32 design studio from NXP and was able to flash my
S32K3x4-Q257 board.
Also I was able to install the MBD toolbox, but it fails during the license check.
Since Linux does not have "vol" command I used my Ethernet address to generate license file.
However it always fails license check... I noticed that at NXP_MBDToolbox_S32K3xx/tools/mlt/ folder only has *.exe files that would not work in Linux.
Is there any way to use it with Linux? Toolchain seems to be compatible, only license activation is the problem!
 
					
				
		
 Irina_Costaches
		
			Irina_CostachesHi @Nomados,
The Model-Based Design Toolbox is a product developed and tested on Windows only, so, unfortunately, the Linux OS is not supported. For more details about the MBDT system requirements, you can consult the Model_Based_Design_Toolbox_S32K3xx_Series_Quick_Start_Guide document.
Regards,
Irina