Hello,
i have a doubt regarding the license needed for the MBDT for Matlab.
On the download page when i click on licenses for the MBDT HCP for the S32G board there is no license available for the 1.3.0 version. Only for the 1.2.0 version.
Does this work for both?
Thank you for your help in advance.
Solved! Go to Solution.
Hi, @monchito911,
If the generated license is valid, it also works for the newer version of the toolbox. A single MBDT license associated with a single machine can be generated for each NXP account. Only if you change your computer you should return and generate another license for the new computer, but as long as you use the same computer, the generated license should work.
Best regards,
Dragos
Hi, @monchito911,
If the generated license is valid, it also works for the newer version of the toolbox. A single MBDT license associated with a single machine can be generated for each NXP account. Only if you change your computer you should return and generate another license for the new computer, but as long as you use the same computer, the generated license should work.
Best regards,
Dragos