Hello,
I'am using
I try to build the gpio_s32k144 example in order to use it with S32K144EVB. I have the following issue:
### Build procedure for model: 'gpio_s32k144' aborted due to an error.
For S-function 'gpio_s32k14_output', the number of defined parameters, 4, does not match the number of parameters on the dialog of 'gpio_s32k144/Digital_Output', 0. These two values must be identical.
Component:Simulink | Category:Block diagram error
For S-function 'gpio_s32k14_output', the number of defined parameters, 4, does not match the number of parameters on the dialog of 'gpio_s32k144/GREEN_LED', 0. These two values must be identical.
Component:Simulink | Category:Block diagram error
For S-function 'gpio_s32k14_input', the number of defined parameters, 6, does not match the number of parameters on the dialog of 'gpio_s32k144/SW2', 0. These two values must be identical.
Component:Simulink | Category:Block diagram error
Could you please tel me what i need to do ? thanks in advance
Regards
Hello Maruis,
Could you please tell me how to declare the environment Variable named "GCC_S32K_TOOL".
is it a command to type on matlab ?
Thanks in advance. Regards
 
					
				
		
 mariuslucianand
		
			mariuslucianand
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello m.benderradji@outlook.fr,
For adding an environment variable in Windows you need to right click Computer -> Properties -> Advanced system Settings and in the Advanced tab you click the "Environment Variables". Then press New... and add the GCC_S32K_TOOl variable name and the compiler location. After that restart Matlab and it will use the new compiler.
Best regards,
Marius
Hello Marious,
Could you please tell me where i can find the steps to follow in order to setup the compilerr for MBDT 2018.R1
I want to use the requested compiler instead of the default one "GCC 6.3 compiler" i think.
Thanks in advance for your support
 
					
				
		
 mariuslucianand
		
			mariuslucianand
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello m.benderradji@outlook.fr,
To use another GCC compiler it is enough to declare an Environment Variable named "GCC_S32K_TOOL" to the location where the GCC complier is installed and restart Matlab after that. If no variable is declared the MBDT uses the default compiler located at "C:\Users\[...]\Documents\MATLAB\Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\code\tools\gcc-6.3-arm32-eabi"
Best regards,
Marius
Thanks Marius
IIs it possible to use Model BaseD Design toolbox without Embedded coder from mathworks ? Is it possible to use only with Matlab coder and Simulink coder ?
Best regards
 
					
				
		
 mariuslucianand
		
			mariuslucianand
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello m.benderradji@outlook.fr,
It is not possible to use the MBDT toolbox without Embedded Coder.
Marius
Hello Marius,
Thank you for your support.
I did not install the old version of MBDT. would you tell me if the issue comes from the installation of the "Motor Control Toolbox supporting S32K"
I'have installed this tool box with the pervious one (MBDT 2018 R1).
Best regards
 
					
				
		
 mariuslucianand
		
			mariuslucianand
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello m.benderradji@outlook.fr,
Please uninstall the "Motor Control Toolbox supporting S32K" and use only "Model-Based Design Toolbox for S32K1xx Series". All the features from that toolbox are embedded in 2018.R1. For a clean install you can follow my previous responses.
Best regards,
Marius
 
					
				
		
 mariuslucianand
		
			mariuslucianand
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello m.benderradji@outlook.fr,
Have you installed the 2018.R1 over the last MBDT version?
Please reset the Matlab "Set Path" to "Default" like in the attached image and then perform a clean install of the MBDT 2018.R1.
Best regards,
Marius
Hello and thanks for your support.
I have already installed the 2018.R1. I have this issue with this last version.
What do you mean by "perform a clean install of the MBDT 2018.R1" after "set path"
Thank in advance for your replay
regards
 
					
				
		
 mariuslucianand
		
			mariuslucianand
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello m.benderradji@outlook.fr,
I assumed that you used the old toolbox version before and the files from the last toolbox version were still in the Matlab's path. So with a clean install I want to be sure that the only files related with the MBDT toolbox are the ones from the current toolbox.
Now, you set the paths to default, go to the Addons folder which typically is C:\Users\[...]\Documents\MATLAB\Add-Ons and in the MBDT toolbox please run the "mbd_s32k_path.m" script.
Now, if you type the command "ver" in the Matlab Command Window, you need to be sure that you have only one toolbox related with S32K. For example I only have this "Model-Based Design Toolbox for S32K1xx Series Version 2018.R1 (R2016b-R2018a)".
Hope this helps,
Marius