Install MBD Toolbox for S12ZVMx, License Error: -9, Model-Based Design Toolbox License Invalid

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Install MBD Toolbox for S12ZVMx, License Error: -9, Model-Based Design Toolbox License Invalid

跳至解决方案
3,346 次查看
gary_lu1
Contributor II

When I install MBD Toolbox for S12ZVMx in matlab R2020a ,it always reported License Error: -9, Model-Based Design Toolbox License Invalid.I checked the version of MATLAB and toolbox,also read all community ways,still can not solve problem.Some information as follows:

1.Matlab version is R2020a,and MBD toolbox is S12ZVMx V1.4.0.

2.Host ID is F4-8E-38-B2-70-C3

3.MBD Demo can open but can not run,reported  license invalid,simulink library can not find the tool box. 

4.I can find toolboxs have been installed in addition function.

5.License path located in ...Toolboxes\NXP_MBDToolbox_S12ZVMx\lic  

Could you help us solve the problem?Thanks.

0 项奖励
回复
1 解答
3,292 次查看
gary_lu1
Contributor II

I‘ve solved this problem,the root cause is that host ID of license not correct,we can not get correct license if we through mac address as host ID.But the toolbox install guidline no to remind it !!! 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,309 次查看
tarafoster
Contributor I

The License Error: -9 for the MBD Toolbox for S12ZVMx in Matlab R2020a is indicating that there is an issue with the license file. Here are some potential solutions to try:

  1. Check that the license file is located in the correct directory: ...Toolboxes\NXP_MBDToolbox_S12ZVMx\lic

  2. Ensure that the license file is named "license.dat" and that it contains the correct Host ID (F4-8E-38-B2-70-C3 in your case).

  3. Verify that the license file has been properly installed by running the "lmutil" command in a command prompt and checking that the S12ZVMx license is listed.

  4. Try restarting Matlab and/or the license server to see if that resolves the issue.

  5. If none of the above solutions work, you may need to contact the software vendor or your IT department for further assistance.

0 项奖励
回复
3,293 次查看
gary_lu1
Contributor II

I‘ve solved this problem,the root cause is that host ID of license not correct,we can not get correct license if we through mac address as host ID.But the toolbox install guidline no to remind it !!! 

0 项奖励
回复