I want to know why it's error for mbd_s32k14_examples

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to know why it's error for mbd_s32k14_examples

1,222 Views
pingli
Contributor III

Dear,all

   why it's error for mbd_s32k14_examplespastedImage_1.png

why it's error for mbd_s32k14_examples,I had no change nothing.

and I've seen the FRDM-S32K144 Freedom board mentioned in a few places, but I can't find it anywhere.

 

Can you provide any info on availability?

thanks,

Clipping Lee

0 Kudos
Reply
2 Replies

949 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi pingli‌,

Have you managed to fix the issue ?

Best regards,
Daniel

0 Kudos
Reply

949 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi pingli‌,

First of all, sorry for delays but your questions have been initially posted into another community.

Your issue looks very much the same with this one:  Something wrong happens when starting SIL or PIL simulation 

As you can see for the your error message, your Operation System does not recognize the spaces in the path and it is splitting the "Program Files" into 2 separate paths that does not exist.

One simple thing to try would be to install the toolbox into C:\NXP\MBDToolbox folder.

If that error still persist then you might need to have a loop of the thread mention above and enable the 8dot3 option

Regarding the second question: are you looking for this one: S32K144 Evaluation Board|NXP 

Hope this helps!

Daniel

0 Kudos
Reply