How to make bootloader image for KV5x from MBDT Matlab

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to make bootloader image for KV5x from MBDT Matlab

1,924 次查看
macphong
Contributor I

Hello everyone,

How can I make bootloader aplication image using NXP MBDT and update this image with "Kinetis Flash Tool" into my TWR-KV58 board?

0 项奖励
回复
4 回复数

1,919 次查看
nxa11767
NXP Employee
NXP Employee

Hi @macphong ,

 

You cannot build an flashloader image from Simulink. But you can find the need files/scripts for this in the SDK of the TRW-KV5x board. You can download the full from nxp site: https://mcuxpresso.nxp.com/en/builder?hw=TWR-KV58F220M 

nxa11767_1-1631270848912.png

And in SDK_2_8_0_TWR-KV58F220M\middleware\mcu-boot\bin you can find some scripts to create a new flashloader and also in Tools the Kinetis Flashing tool.

nxa11767_2-1631271134189.png

 

I hope this helps,

Alexandra

 

 

 

0 项奖励
回复

1,912 次查看
macphong
Contributor I

Hi,

I've already done my project using bootloader with KeilC, I only modified project from example direction ".\SDK_2.8.0_TWR-KV58F220M\boards\twrkv58f220m\bootloader_examples\demo_apps\led_demo_tower_a000" and using the .hex or .bin file. Now, I want to do it with MBDT from Simulink on my current Project, It's disappointed to heart that cannot build from Simulink

0 项奖励
回复

1,883 次查看
nxa11767
NXP Employee
NXP Employee

Hi @macphong ,

 

I had the impression that you want to build the flashloader itself from Simulink, but you want to create an normal application that will be loaded using the flashloader. Is a feature that can be added in the next release of the KVx toolbox. Currently  the application is build to be loaded via PE Micro or Jlink probe. We plan an update for the MBDT for KV series somewhere in Q2 next year, that will add the missing peripherals and also we can include this method of building and loading the application via flashloader. Please let me know if you need an early patch with just this feature.

Best regards,

Alexandra

0 项奖励
回复

1,872 次查看
macphong
Contributor I

Hi @nxa11767 ,

Thanks for your help and if you dont mind, please let me know if you have new patch or trial version about flashloader and some peripheral as CAN, HSADC, flexPWM.

My email: macluuphong.ct@gmail.com

Thank you & best regard,

Phong

0 项奖励
回复