How to go to the following path as shown in Quick start guide

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to go to the following path as shown in Quick start guide

2,123 Views
sutter_zhou
NXP Employee
NXP Employee

sutter_zhou_0-1619703546511.png

 

0 Kudos
Reply
3 Replies

2,114 Views
sutter_zhou
NXP Employee
NXP Employee

I'm not talking about the simulink library page. It is the left side of this picture that makes people confused. People need to navigate to a specific path to see this folder structure.

sutter_zhou_0-1619706277727.png

 

0 Kudos
Reply

2,099 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @sutter_zhou,

Sorry, my bad! All the MBDT toolboxes are installed in the MATLAB AddOns specific folder, which may differ for each user (everyone can select his own). To find your own or to change the default one, go to MATLAB -> Preferences and under Add-Ons you may find the toolbox location.

mariuslucianand_0-1619723869774.png

 

But, once the I.MXRT toolbox has been installed, you can type the following command in MATLAB's Command window: cd(mbd_find_imxrt_root) and this will change the Current Workspace to the one from the image.

Hope this helps,

Marius

0 Kudos
Reply

2,117 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @sutter_zhou ,

If you refer to the Simulink library browser, you have 2 options to see it:

1. Go in any Simulink model, and you should find it under SIMULATION > Library Browser

mariuslucianand_1-1619705397065.png

2. type slLibraryBrowser in MATLAB Command Window

mariuslucianand_0-1619705258435.png

If you have installed the Toolbox but anything is missing, you can refresh the library by pressing the F5

Hope this helps,

Marius

0 Kudos
Reply