How to drive S32K144EVB correctly In Matlab simulation environment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to drive S32K144EVB correctly In Matlab simulation environment

5,720件の閲覧回数
chen2021
Contributor I

Hello

In Matlab simulation environment.
I plan to use microUSB to update the model of S32K144EVB.
I updated a few examples,and there are no errors in the diagnostic viewer.
But EVB is unexecuted the model.
Could you give me some instructions? please

Two target connection settings are used(attachment:1.GPIO LED Blink(COM9).PNG & 2.GPIO LED Blink (OPEN SDA).PNG)
Installed the driver(attachment:3.DRIVER.PNG)
EVB appearance(attachment 4:.EVB.jpg)

0 件の賞賛
返信
3 返答(返信)

5,709件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @chen2021 ,

Can you please check if the Download Code after Build option is checked?

mariuslucianand_0-1626979659419.png

Hope this helps,

Marius

 

0 件の賞賛
返信

5,700件の閲覧回数
chen2021
Contributor I

@mariuslucianand 

Hello Marius

Thanks for your reply.

Yes, it has been checked, but still unable to successfully update the model to EVB.

Setup screenshot as attachment

 

0 件の賞賛
返信

5,588件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @chen2021 ,

Can you please try to copy paste manually the .mot file form the generate folder to the mounted disk drive of the board? Maybe the OpenSDA needs an update on the board as described here https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Update-OpenSDA-Firmware-on-EVB/t...

Hope this helps,

Marius

 

 

0 件の賞賛
返信