It depends on which compiler you are using.
If you are using GCC you need to replace line 450
$(ELF_TOOL) -O srec $(MODEL).elf $(MODEL).mot
with
$(ELF_TOOL) -O binary $(MODEL).elf $(MODEL).bin
For GCC you have the following options:
srec Save as Motorola S-records
   $(ELF_TOOL) -O srec $(MODEL).elf $(MODEL).s19
binary  Save as raw binary
   $(ELF_TOOL) -O binary $(MODEL).elf $(MODEL).bin
ihex     Save as Intel hex
$(ELF_TOOL) -O ihex $(MODEL).elf $(MODEL).hex
If you are using IAR you replace line 453
$(ELF_TOOL) $(MODEL).elf $(MODEL).mot --srec --silent
with
$(ELF_TOOL) $(MODEL).elf $(MODEL).bin --bin --silent
For IAR you have the following options:
--srec Save as Motorola S-records
   $(ELF_TOOL) $(MODEL).elf $(MODEL).s19 --srec --silent
--ihex          Save as Intel hex
   $(ELF_TOOL) $(MODEL).elf $(MODEL).hex --ihex --silent
--bin            Save as raw binary
$(ELF_TOOL) $(MODEL).elf $(MODEL).bin --bin --silent
ATTENTION: Lines 450 and 453 should start with a tab.
I see that you are using the old version of toolbox, MCToolbox for S32K, you can get for free the new version, MBDToolbox for S32K from NXP Motor Control Toolbox
powerpc-eabivle-objcopy
If you want to automate it put it in the _make_rtw_hook.m callback.
See also:
Converting S19 Files into Binary Files with GNU objcopy | MCU on Eclipse
用MBD工具箱生成的elf文件,然后下载到板子上。现在我想知道怎么设置,能够生成bin/hex/s19文件~~~
Hello,
The easiest way to achieve your goal is to modify the default settings in the mbd_s32k14.tmf file within c:\MBDToolbox\mbdtbx_S32K\mbdtbx_s32k14\mbdtbx_s32k14\ folder
This file is responsible for generation the makefile used to build the model.
Inside the file, there is already a default example about how to generate a SREC from the elf. Therefore is a simple as changing the extension and the type of file you want to obtain: bin/hex/s19 etc since the toolchain is defined already.
Step1: search for any occurrences of ".mot" keyword
Step2. replace with the ".extension_you_want_to_obtain"
Step3: find the invocation of ELF_TOOL
Should look like this:
$(MODEL).mot: $(MODEL).elf
 @echo Generating S-record...
ifeq ($(TARGET_COMPILER), GCC)
 $(ELF_TOOL) -O srec $(MODEL).elf $(MODEL).mot
endif
ifeq ($(TARGET_COMPILER), IAR)
 $(ELF_TOOL) $(MODEL).elf $(MODEL).mot --srec --silent
endif
ifeq ($(TARGET_COMPILER), GreenHills Multi)
 $(GSREC_TOOL) -auto -o $(MODEL).mot $(MODEL).elf
endif
 @echo Created S-record: $(MODEL).mot
And replace it with something like this:
$(ELF_TOOL) -O binary $(MODEL).elf $(MODEL).bin
Hope it helps!
Daniel
只需要改如图的两行是把。只需要改后缀?中间的srec需要改吗?如果我想改成S19文件,应该怎么改?
Hello,
We're making efforts to understand Chinese as much as we can with Google Translate but sometimes that fails. In this case using the translate function i can't understand what are you asking.
Can you please rephrase in English.
Thank you!
Daniel
Hello,
sorry,my English is very bad.Can you help me to creat .s19 file in IAR .thank you very much.
It depends on which compiler you are using.
If you are using GCC you need to replace line 450
$(ELF_TOOL) -O srec $(MODEL).elf $(MODEL).mot
with
$(ELF_TOOL) -O binary $(MODEL).elf $(MODEL).bin
For GCC you have the following options:
srec Save as Motorola S-records
   $(ELF_TOOL) -O srec $(MODEL).elf $(MODEL).s19
binary  Save as raw binary
   $(ELF_TOOL) -O binary $(MODEL).elf $(MODEL).bin
ihex     Save as Intel hex
$(ELF_TOOL) -O ihex $(MODEL).elf $(MODEL).hex
If you are using IAR you replace line 453
$(ELF_TOOL) $(MODEL).elf $(MODEL).mot --srec --silent
with
$(ELF_TOOL) $(MODEL).elf $(MODEL).bin --bin --silent
For IAR you have the following options:
--srec Save as Motorola S-records
   $(ELF_TOOL) $(MODEL).elf $(MODEL).s19 --srec --silent
--ihex          Save as Intel hex
   $(ELF_TOOL) $(MODEL).elf $(MODEL).hex --ihex --silent
--bin            Save as raw binary
$(ELF_TOOL) $(MODEL).elf $(MODEL).bin --bin --silent
ATTENTION: Lines 450 and 453 should start with a tab.
I see that you are using the old version of toolbox, MCToolbox for S32K, you can get for free the new version, MBDToolbox for S32K from NXP Motor Control Toolbox