How can we tell processor MC8640TVU1067NE is working fine or not???

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can we tell processor MC8640TVU1067NE is working fine or not???

1,401 次查看
phanikumarkorla
Contributor I

Hi all,

A. From the processor (MC8640TVU1067NE ) the bus address (BA) signals is not coming as per expected. Those lines is directly going to DDR Ic's only. because of those signals Bsp flashing is not happening what could be the reason processor or DDR Ic's. Actually we are using 4DDR Ic's so all DDR Ic's won't go bad at a time. please suggest me to to find out faulty Ic, one more thing all input signals which need to go for IC is reaching fine.

B. From DDR ic (part number: mt47h128m16hg-3it:a) data out line's is coming less voltage. According to data sheet of that IC the out voltage should be 1.6 to 1.8v but IAM getting 1.2v. The reason might be DDR ic only or processor only.

标签 (3)
标记 (1)
0 项奖励
回复
1 回复

1,237 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi phanikumarkorlapati‌,

This is SW community providing support for MATLAB related toolboxes. Unfortunately we do not have anything in our tool-bag to address your requests. My advice is to get in touch with NXP's Support via ticketing system in order to have your question routed to the appropriate team that might address your use-cases: 

https://nxpcommunity.force.com/community/ 

Hope this help!

Daniel

0 项奖励
回复