Freemaster with MPC5744P: can not detect the board information

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freemaster with MPC5744P: can not detect the board information

3,024 Views
13226508
Contributor III

Hi,everyone,

   When I try to implement the " MotorControl_0_pnt.mdl ", the FreeMaster will error that "can't detect the board information"(AS shown below).But I do a little bit modify to the model,  when I remove the part circled by blue, the freemaster and 5744p could communincation correctly. When I add it, the Freemaster won't work properly. 

    My matlab version is 2016a, and S32DS version is 2017.R1,Freemaster version is 2.0

pastedImage_1.png

pastedImage_2.png

0 Kudos
Reply
2 Replies

2,757 Views
mariuslucianand
NXP Employee
NXP Employee

Hello 13226508@qq.com‌,

I think your problem is related with this one https://community.nxp.com/thread/513398  so please start using our latest release or try some suggestions from that topic.

Hope this helps,

Marius

0 Kudos
Reply

2,757 Views
13226508
Contributor III

Hi,Marius,

   I did it as you said, but the problem remained unsolved.Do you have any other suggestions?

Regards,

0 Kudos
Reply