Evaluate Resolver and Generate PWM in MBDT without eTPU - MPC5775E

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Evaluate Resolver and Generate PWM in MBDT without eTPU - MPC5775E

2,203件の閲覧回数
TLin3
Contributor III

Hello NXP MBDT Community,

I would like to develop motor control application software for a MCSPTR2A5775E motor DevKit with MPC5775E board using the MBDT.

Two essential functions, resolver feedback and three-phase PWM output signals, are using the eTPU. The MBDT does not have feature blocks/functions set up the eTPU-related functions.

Here is the same topic, but did not get the support to have those two functions achieved successfully.


https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5775E-Generate-PWM-and-Evaluate-Reso...

 

Would you please kidly support this topic, please?

Thanks

0 件の賞賛
返信
3 返答(返信)

2,066件の閲覧回数
TLin3
Contributor III

Hello NXP MBDT Community,

Anyone could support this topic, please?

Thanks

0 件の賞賛
返信

2,156件の閲覧回数
victormarcel036
Contributor I

MCSPTR2A5775E motor DevKit with the MPC5775E board using MBDT. It seems that you are facing challenges with setting up the resolver feedback and three-phase PWM output signals using the eTPU. I apologize for the lack of support you received previously. I would be happy to assist you in finding a solution for achieving those two functions successfully. Follow My Health

0 件の賞賛
返信

2,128件の閲覧回数
TLin3
Contributor III

Hi @victormarcel036 ,

Thanks for replying to my message.

Is it possible to achieve these two functions without using eTPU?

Alternatively, if eTPU could work with MBDT, how would it work? 

https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/How-to-use-your-own-C-code-in-our-Toolbox-...

Would you advise, please? 

0 件の賞賛
返信