Error encountered " Complication artifacts are out of date"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error encountered " Complication artifacts are out of date"

1,113 次查看
XH
Contributor I

Hi @FlorinCiuca ,

I hope this message find you well. I was mimicking the Model Based Design Toolbox: ADC PWM example project from the MR-CANHUBK344 library to build the a similar project on S32K358 processor. However, after I deploy the project onto the S32K358, this error message jumped out: "Complication artifacts are out of date", as seen in the attached photo, and the attached error log. Could you please advice me possible ways to solve this issue? Many thanks from Xiaomei

标记 (1)
0 项奖励
回复
1 回复

1,078 次查看
FlorinCiuca
NXP Employee
NXP Employee

Hello @XH !

I analyzed the screenshot and build log that you provided. It seems that the build process ends successfully and the only problem occurs when the download on the board is attempted:

download.png

 Please make sure that the connections between the board, debugger and your laptop/PC are performed correctly. Also, please check in the Model Settings that the proper Download method is selected (please re-visit this article https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Error-Problem-occured-while-downloading...). If the connections are done correctly, the board power supply is fed and the correct download method is selected, your model should work as expected.

 

Best regards,

Florin.

0 项奖励
回复