Error Pil example MBDT S12ZVM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error Pil example MBDT S12ZVM

1,475 次查看
Stefan_9811
Contributor II

Dear all,

 

we installed the Model Based Design Toolbox (MBDT) for S12zvm and tried to run the provided example for the PIL Simulation. Unfortunately we get an error when we try to start the Simulation. 

The steps we take are:

  1. Open model "sim_pil_test_s12zvm"
  2. Select our target and enable pil simulation in the configuration Block
  3. Select Subsystem=>Tools=>NXP Model-Based Design Toolbox for S12zvm => To Pil Mode on Mc9S12ZVM

Unfortunately we still get the attached error. 

We are using the #MC9S12ZVM High current Board with Matlab 2019b and the MinGW64 mex compiler.

Has anyone a suggestion? 

Kind regards.

@paulvlase @Daniel_Popa 

0 项奖励
回复
1 回复

1,365 次查看
paulvlase
NXP Employee
NXP Employee

Hello @Stefan_9811 ,

 

Can you try to apply the attached patch MBDToolbox_S12ZVMx_1.4.0_patch_03072023.exe.zip and run PIL simulation again?

 

Steps to apply the patch:

1. Download the attached zip file and unzip it.

2. Open Matlab and run mbd_find_s12z_root() to get the root folder there the S12ZVM toolbox is installed.

3. Close Matlab.

4. Open the MBDToolbox_S12ZVMx_1.4.0_patch_03072023.exe.zip file and extract it's contents to the root folder of the toolbox.

 

Regards,

Paul

0 项奖励
回复