EmiosCommon Settings Greyed out

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EmiosCommon Settings Greyed out

ソリューションへジャンプ
899件の閲覧回数
Vast-Horizon
Contributor II

Hello,

VastHorizon_2-1714163555707.png

 

I'm trying to use PWM to control the intensity of the red LED on the S32K358, so I try to follow section 4 of this tutorial:

https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Controlling-LED-intensity-with-ADC-and-PWM...

Like the tutorial 4.3, I set the Emios to enable  via Mcu -> McuModuleConfiguraion ->McuModeSettingConf - >McuPeripheral

VastHorizon_4-1714163967629.png

 

But my EmoisCommon settings are greyed out:

VastHorizon_0-1714163464359.png

I'm not sure what to do now. Without the EmoisCommon config, it's giving me the error on PwmemiosBufsRef

VastHorizon_3-1714163595548.png

Can anyone help me out? Thanks.

 

 

タグ(3)
0 件の賞賛
返信
1 解決策
869件の閲覧回数
Irina_Costachescu
NXP Employee
NXP Employee

Hi @Vast-Horizon 

For being able to configure Emios settings inside Mcl, you should have the following check enabled inside the Mcl General Configuration tab, as illustrated below.

Irina_Costachescu_0-1714388246419.png

Hope this helps,

Irina

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
870件の閲覧回数
Irina_Costachescu
NXP Employee
NXP Employee

Hi @Vast-Horizon 

For being able to configure Emios settings inside Mcl, you should have the following check enabled inside the Mcl General Configuration tab, as illustrated below.

Irina_Costachescu_0-1714388246419.png

Hope this helps,

Irina

 

0 件の賞賛
返信