EmiosCommon Settings Greyed out

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EmiosCommon Settings Greyed out

Jump to solution
902 Views
Vast-Horizon
Contributor II

Hello,

VastHorizon_2-1714163555707.png

 

I'm trying to use PWM to control the intensity of the red LED on the S32K358, so I try to follow section 4 of this tutorial:

https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Controlling-LED-intensity-with-ADC-and-PWM...

Like the tutorial 4.3, I set the Emios to enable  via Mcu -> McuModuleConfiguraion ->McuModeSettingConf - >McuPeripheral

VastHorizon_4-1714163967629.png

 

But my EmoisCommon settings are greyed out:

VastHorizon_0-1714163464359.png

I'm not sure what to do now. Without the EmoisCommon config, it's giving me the error on PwmemiosBufsRef

VastHorizon_3-1714163595548.png

Can anyone help me out? Thanks.

 

 

Tags (3)
0 Kudos
Reply
1 Solution
872 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hi @Vast-Horizon 

For being able to configure Emios settings inside Mcl, you should have the following check enabled inside the Mcl General Configuration tab, as illustrated below.

Irina_Costachescu_0-1714388246419.png

Hope this helps,

Irina

 

View solution in original post

0 Kudos
Reply
1 Reply
873 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hi @Vast-Horizon 

For being able to configure Emios settings inside Mcl, you should have the following check enabled inside the Mcl General Configuration tab, as illustrated below.

Irina_Costachescu_0-1714388246419.png

Hope this helps,

Irina

 

0 Kudos
Reply