Hi Daniel,
I'm having the same issue as David.
"Can not detect board information ! (...) [ERROR code=0x80000101]" when starting Ctrl+F, after arranging the Project Options according to the QuickStart manual.
Running Connection Wizard -> Use direct connecxtion to on-board USB port ->UART: COM3 OpenSDA+ 115200/9600 Baud-rate results in Error: "No board detected on any of specified UART communication ports."
Hardware Information:
Board Name is: EVB-S32K144
MicroBoot Kernel Version is: 1.08
Bootloader Version is: 1.11 -> this was 1.13 out of the box IIRC (but that didn't work either)
Installed Application: PEMicro EVB-S32K144 Mass Storage/Debug App
Application Version is: 1.19
The application is the OOBE -> LED RGB Toggling. It is working from the beginning.
Software:
OS: Windows 10 Pro, Version: 1803
FreeMASTER 2.0.8.0 (comm.protocol v3+)
Steps I made to try and fix the connection problem:
- Manually installing PEMicro Drivers from their OpenSDA Support (after FreeMASTER didn'T recommend a COM)
- Trying FreeMaster 1.4
- Updating Bootloader: BOOTUPDATEAPP_Pemicro_v111.SDA
- Updating MSD: MSD-DEBUG-EVB-S32K144_Pemicro_v119.SDA
Nothing helped.
Do you need any further information?
How to get FreeMASTER embedded Driver support onto my s32k144EVB?
Best regards,
Tim