Difference btw SIL and PIL due to an error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Difference btw SIL and PIL due to an error

7,810 次查看
ykarata1
Contributor IV

Hello everyone,

I have a complex Simulink model on my computer. When I want to use SIL, i can make it operate. It works great.

When I convert it to PIL, it gives me, error that I have shared related image below. By having in my mind that I can make a simple PIL model in the same processor and using same configuration in both simple and complex model, I do not think that Causes a and b is not the problem.

I think Cause c is the real problem here. If so,

Since C code is generated in SIL also, What is the problem with PIL? Both generates C code and implement it. SIL operates C code on my computer, PIL operates C code on Processor. 

For detecting subsystems that prevent PIL from operating, I created a blank model and added subsystem of complex model one by one and tried PIL method for each step. My goal was detecting subsystems that is not suitable with PIL. But I have an enormous model and that takes a lot of time. Also since PIL has it own rules, it takes great effort at each step.

My Questions here are:

1. Why PIL do not operate while same model operate succesfully at SIL ?

2. How can I learn, debug easily which subsytem causes PIL to not work ?

Thanks.

pastedImage_4.png

标记 (3)
10 回复数

7,458 次查看
constantinrazva
NXP Employee
NXP Employee

Hello ykarata1@ford.com.tr ,

I understand your frustration, but there is no simple answer I can give on why it is not working in PIL mode. The timeout can be caused by more factors so it would be helpful if you could give us more details regarding the model: are you using any peripheral blocks? Are you using blocks for interrupts? Do you know if the application has crashed? (here it might be helpful if you had an LED blinking just to let you know if it's still working).

While SIL is code generated on your computer, when it comes to PIL there are other factors that come in play - such as the connection between the MCU and the PC where you are running Simulink. Sometimes this causes an issue; other times, interrupts are getting in the way of this or better yet, sometimes interrupts are enabled on a certain peripheral that was not yet configured, and that causes the application to crash. This are just a few things that come to mind when talking about PIL issues.

paulvlase‌ has a lot more expertise on this subject, so he can assist you further. I know that I have not answered fully your question, I just tried to let you know a few factors that may lead to this.

Kind regards,

Razvan.

0 项奖励
回复

7,460 次查看
ykarata1
Contributor IV

Dear constantinrazvan.chivupaulvlase‌,

Thanks for your effort. I am trying to solve the problem still.

I also focused on timeout. I tried to change timeout by changing ConnectivityConfig. But despite of changing it, I got the error and error still says that timeout is still 10 seconds.

a.jpg

b.jpg

From that, I understand that I could not change timeout. Also I have looked for local project file to find that timeout value to change.

Thanks.

7,460 次查看
constantinrazva
NXP Employee
NXP Employee

Hello ykarata1@ford.com.tr ,

I suspect the timeout is just an effect, not the cause. There might be something that crashes the application; 10s should be enough to start the connection between Simulink and the target.

Maybe you could share your model so we can test it on our end - if you have proprietary code, either strip it down to a bare minimum to reproduce the error, either you can send it in a private email. It makes it easier for us to get to the bottom of things if we can test it on our end.

Kind regards,

Razvan.

7,460 次查看
ykarata1
Contributor IV

Dear constantinrazvan.chivu‌,

We have talked the issue with MATLAB personals.

They have mentioned that they had solved the problem by increasing timeout value in the past. So It think it worth to try at least. If that does not solve out problem we may evaluate sharing our model with you.

My question here:

1. Why when I increase timeout in ConnectivityConfig, timeout still stays at 10 second?

2. How can I change timeout value?

Matlab personal has told us that we can increase timeout by changing line that is written in the Processor xml from 10 to something more. But there is not any line on MPC processor xml. I guess NXP follow a different structure on that.

<externalmodelinfo preconnectfcn="pause(10)">

Thanks.

0 项奖励
回复

7,460 次查看
paulvlase
NXP Employee
NXP Employee

Hi ykarata1@ford.com.tr‌,

You changed the PIL communication timeout in the AUTOSAR PIL ConnectivityConfig.m file.

If you are not developing an AUTOSAR application, you have to change that timeout in

fullfile(mbd_find_mpc_root(), 'mbdtbx_mpc574x', 'mbdtbx_mpc574x', '+mpc574x_pil', 'ConnectivityConfig.m')

Run this command in the Matlab console to get the full path.

Are you able to run our simple PIL simulation example, sim_pil_top_mpc574x.mdlsim_pil_top_mpc574x.mdl, found in fullfile(mbd_find_mpc_root(), 'MPC_Examples', 'common', 'pil')?

Were you able to run PIL simulation for the blank model with only the MBD_MPC574x_Config_Information block in the model?

Can you post a screenshot of the Target Connection tab from the MBD_MPC574x_Config_Information block from your model?

Do you have referenced models in your application?

The Matlab guys are referring to the custom target approach to tell Simulink for which target it is generating the code, how to build it and run it in the board using xml files. We are planning to move to this approach, but right now we are using another one, so there are no xml files to change. You can change the PIL communication timeout only from ConnecitivityConfig.m files.

Regards,

Paul

7,460 次查看
ykarata1
Contributor IV

Dear paulvlase and constantinrazvan.chivu,

1. I only have .p files which I can not see its inside and change it. As far as I understood they are coded and can not be decoded.

pastedImage_1.png

2. I can succesfully run sim_pil_top_mpc574x.mdl.

pastedImage_2.png

Figure 3: Target Communication of my model

pastedImage_3.png

Thansk.

0 项奖励
回复

7,452 次查看
paulvlase
NXP Employee
NXP Employee

Hi ykarata1@ford.com.tr‌,

Oops! I forgot to check if non-autosar ConnectivityConfig is pcode in the mltbx. Delete ConnectivityConfig.p and use the attached ConnectivityConfig.m instead.

The settings from the Target Connection look good. Can you try to lower the Baud Rate to 57600?

As constantinrazvan.chivu‌ told you already, it would be easier and faster if you could send us a simplified version of your model to us as a reply to the e-mail that I sent to you.

.

Regards,

Paul

7,452 次查看
ykarata1
Contributor IV

Dear All paulvlase and constantinrazvan.chivu,

Thanks for your great effort.

We have changed timeout by ConnetivityConfig.m file that you have sent but problem exists still. Hopefully we have eliminated one possible cause.

We do not know why PIL does not work while SIL works.

Thanks again.

0 项奖励
回复

7,452 次查看
constantinrazva
NXP Employee
NXP Employee

Hello ykarata1@ford.com.tr ,

The line you changed in the ConnectivityConfig.m file was the correct one - maybe there are issues with the message being displayed -- let me check it out and I'll get back on this.

EDIT: the file name is correct, but you changed it for AUTOSAR -- you can find the correct one in {TOOLBOX_ROOT}\mbdtbx_mpc574x\mbdtbx_mpc574x\+mpc574x_pil

[Thank you paulvlase‌ for pointing it out]

Kind regards,

Razvan.

3,799 次查看
adr3psch
Contributor I
Hi, I am facing a similar issue with an NXP S32K144, would you be able to share the ConnectivityConfig.m for this board? I have a predictoin algorithm that runs fine up to 10s of prediction horizon, but for horizons higher than that I get the timeout error. It runs fine on SIL though.
0 项奖励
回复