Device is not detected or may be censored. DEVKIT-MPC5748G

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Device is not detected or may be censored. DEVKIT-MPC5748G

2,110件の閲覧回数
60010001
Contributor II

I follow Model Based Design Toolbox MPC57xx Series Quick Guide .In Bootloader Setup ,I used S32DS.POWER.2.1 to flash bootloader but it showed Device is not detected or may be censored then i follow this uncensorpassword  but nothing change it has same problem. 

My previous post ,i can't see the answer .

I’m very sorry I have troubled you.Screenshot (279).pngScreenshot (278).pngScreenshot (277).pngScreenshot (276).pngIMG_20200704_145330.jpg

0 件の賞賛
4 返答(返信)

1,942件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello 60010001@kmitl.ac.th‌,

Can you please attach an image with the board connected to the PC? I am interested in which LEDs are lighting and how the jumpers are set.

Thanks,

Marius

0 件の賞賛

1,942件の閲覧回数
60010001
Contributor II

In this question,I forgot to change J11 to 2,3

IMG_20200707_175432.jpg

but when i changed J11 to 2,3 i have this problem

IMG_20200707_175200.jpgScreenshot (285).png

0 件の賞賛

1,942件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello 60010001@kmitl.ac.th‌,

It seems there are two revisions for the MPC5748G board: reb B and rev D. From the images you have attached I see that you own the rev D. 

Anyway, basically the J11 sets the power source and if you try to power the board only for the computer, then you have to set it on the position 2-3. The two LEDs that are turned on, specifies that the voltages 3V3 and 5V are ok.

 https://www.nxp.com/docs/en/quick-reference-guide/DEVKIT-MPC5748G-QSG.pdf  

pastedImage_2.png

Leave it on the position 2-3 if you are only powering the board over the uUSB and try flashing the bootloader on the board. The target seems to be detected now so please, retry a Simulink model over the PC8 and PC8 of the LinFlex2 serial. 

pastedImage_3.png

Hope this helps,

Marius

0 件の賞賛

1,942件の閲覧回数
60010001
Contributor II

I use embedded coder for build code to the board but it occur like this

Screenshot (286).png

before this i try to flash bootloader with this file

Screenshot (287).pngScreenshot (285).png

0 件の賞賛