DMA configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DMA configuration

1,049 次查看
juliana_rojas30
Contributor III

Hello!

I have some questions regarding the implementation of the DMA blocks in my system. I implemented a model in which I use DMA to echo back CAN messages that I received in my board. 

1. I've not been able to find the correct registers to configure the block for "edma transfer", can I get support on this? I've included the DMA blocks for doing the following procedure:

Receives over CAN -> I put message received in 0x20000000

eDMA copies from 0x20000000 to 0x20000001

I read message copied from 0x20000000 -> I send over CAN again

 2. I want to calculate the processor load of the model with a DMA included. Would the calculations I specified here work for a model with DMA? In case it doesn't, is there a way to know how much processor load is using the model in this DMA case? I know the result should be very low, but I want to be certain of the correct implementation of the blocks by observing this parameter.

Thanks.

Kind regards.

0 项奖励
回复
0 回复数