I’m trying to use the NXP_Support_Package_BMS Add-On for MBDT, which is officially supported for S32K3xx MBDT v1.4.0.
My system already has MBDT v1.5.0 installed for other ongoing projects, but the add-on does not seem to work with this newer version.
I am currently using the S32K396 POC Board for BMS development.
Is there:
- Any method to make the Add-On compatible with v1.5.0, or
- Is there a way to install and run both v1.4.0 and v1.5.0 in parallel on the same MATLAB installation or system without conflicts?
If parallel installation is possible, please guide me on the correct setup steps.