Hi,
As with other I get the following error when adding the Write_Registers block into my model:

Becuase this doesn't work and I can't find anything on the search to fix this, I was wondering whether I can use the DataMemWrite to do the same thing? I need to write a value to IFLAG1 to clear the interrupt. Here it is in the datasheet:

As it has an offset of 30h, can I set up the DataMemWrite block like this, or does this block do something completely different?:


@mariuslucianand Any help is appreciated.
Thank you!