AMCLIB_BemfObsrvDQ function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AMCLIB_BemfObsrvDQ function

1,294 Views
872454246
Contributor II

        Now I need to use MC9S12ZVM to run my motor above the electric speed of 50,000 RPM, but the maximum value of the 16-bit mathematical library is around 32000. Could you please provide the code of AMCLIB_BemfObsrvDQ function for me to modify? Thank you!  I wrote my own code using the model block diagram above AMCLIB_BemfObsrvDQ parameters, but failed.  

0 Kudos
Reply
0 Replies