13/5000 S32K344 CAN communication

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

13/5000 S32K344 CAN communication

754 Views
yu123
Contributor I

hello

I use the MBD case model provided by the official,C code was generated and compiled and written in S32DS software. All the processes were successful. But why did I use other CAN nodes to transmit messages to the development board but failed.Can you help me!

屏幕截图 2022-05-22 205053.png

0 Kudos
2 Replies

693 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @yu123 ,

Are you still facing this issue on the S32K3?

Regards,

Marius

0 Kudos

680 Views
yu123
Contributor I

Hello

Because the blue light is always on after programming, I judged that there is a problem with the modules TJA1153_Init.So I modified the code in the file mbdt_tja1153 and deleted part of the code, assuming there is no problem, the operation is successful.Is this what is the reason?

屏幕截图 2022-06-09 191039.png

屏幕截图 2022-06-09 191105.png

0 Kudos