Hi Zhou ten,
For IAR you need to follow this procedure: IAR Flashing an existing image without risking a re-build
Basically you create a new project by selecting the Externally built executable option:
Then make sure you select the S32K144 as Device from Project Options
Hope this helps!
Daniel
请问你解决了么?我也出现了这个问题。拜托拜托
Hi Daniel :
I have added the executable file into IAR Embedded Workbench ,then debug the project, it appeared error like the picture,could you like to tell me the reason?Thank you very much!
Ni hao,
That's about all the Chinese i know.
I guess you what to know how to use the S32DS or IAR to load the executable file produced with Matlab into the S32K board right ?
If that is the case you can use the elf importer (e.g. S32DS): File/Import/Executable File Importer
Then the wizard will guide you thru the rest of the process.
Best regards,
Daniel
Hi Daniel:
Thank you ,I also want to know how to use the "IAR" to load the executable file produced with Matlab into the S32K board , Because I use the IAR to work recently~
Best regards,
Zhou ten
Hi Zhou ten,
For IAR you need to follow this procedure: IAR Flashing an existing image without risking a re-build
Basically you create a new project by selecting the Externally built executable option:
Then make sure you select the S32K144 as Device from Project Options
Hope this helps!
Daniel
Hi Daniel :
I find that “the IAR” only open ".eww" file.
Hi Zhou ten,
I do not know Chinese, but i think the dialogue you are seeing ask you to save the new project.
Only after you create the IAR project you will be able to load the additional file you wish to debug.
Hope this helps!
Daniel
ok.Thank you very much~~~~