Hi ,
I wrote a sample code (please see the attachment) to use watchdog timer for two roundrabin tasks. when I have only one task (e.g. only simulated_ISR_task_1) it works well but when I add the second task (simulated_ISR_task_2) it stops work. I've check the MQX plugin tool. it didn't show any error or something wrong! any
suggestion?
Regards
#include <mqx.h>
#include <bsp.h>
#include <event.h>
#include <watchdog.h>
/* Task IDs */
#define MAIN_TASK 5
#define ISR_1_TASK 6
#define ISR_2_TASK 7
/* Function prototypes */
extern void simulated_ISR_task_1(uint_32);
extern void simulated_ISR_task_2(uint_32);
extern void main_task(uint_32);
extern void handle_watchdog_expiry_1(pointer);
extern void handle_watchdog_expiry_2(pointer);
const TASK_TEMPLATE_STRUCT MQX_template_list[] =
{
/* Task Index, Function, Stack, Priority, Name, Attributes, Param, Time Slice */
{ MAIN_TASK, main_task, 2000, 8, "service", MQX_AUTO_START_TASK, 0, 0 },
{ ISR_1_TASK, simulated_ISR_task_1, 2000, 9, "simulated_ISR1", MQX_TIME_SLICE_TASK, 0, 1 },
{ ISR_2_TASK, simulated_ISR_task_2, 2000, 9, "simulated_ISR2", MQX_TIME_SLICE_TASK, 0, 1 },
{ 0 } };
/*TASK*-----------------------------------------------------
*
* Task Name : simulated_ISR_task
* Comments :
* This task opens a connection to the event group. After
* delaying, it sets the event bits.
*END*-----------------------------------------------------*/
void handle_watchdog_expiry_1(pointer td_ptr)
{
pointer event_ptr;
_mqx_uint event_bits;
printf("expire_1\n\r");
fflush(stdout);
}
void handle_watchdog_expiry_2(pointer td_ptr)
{
pointer event_ptr;
_mqx_uint event_bits;
printf("expire_2\n\r");
fflush(stdout);
}
void simulated_ISR_task_1(uint_32 initial_data)
{
pointer event_ptr;
MQX_TICK_STRUCT ticks;
_mqx_uint result;
_time_init_ticks(&ticks, 10);
result = _watchdog_create_component(BSP_TIMER_INTERRUPT_VECTOR,
handle_watchdog_expiry_1);
printf(" restart1 \n");
while (TRUE)
{
result = _watchdog_start_ticks(&ticks);
_time_delay(100);
_watchdog_stop();
}
}
void simulated_ISR_task_2(uint_32 initial_data)
{
pointer event_ptr;
MQX_TICK_STRUCT ticks;
_mqx_uint result;
_time_init_ticks(&ticks, 10);
result = _watchdog_create_component(BSP_TIMER_INTERRUPT_VECTOR,
handle_watchdog_expiry_2);
printf(" restart2 \n");
while (TRUE)
{
result = _watchdog_start_ticks(&ticks);
_time_delay(100);
_watchdog_stop();
}
}
/*TASK*-----------------------------------------------------
*
* Task Name : service_task
* Comments :
* This task creates an event group and the simulated_ISR_task
* task. It opens a connection to the event group and waits.
* After the appropriate event bit has been set, it clears
* the event bit and prints "Tick."
*END*-----------------------------------------------------*/
void main_task(uint_32 initial_data)
{
pointer event_ptr;
_task_id task_id_1, task_id_2;
_mqx_uint event_bits;
/* Create the ISR task */
task_id_1 = _task_create(0, ISR_1_TASK, 0);
if (task_id_1 == MQX_NULL_TASK_ID)
{
printf("Could not create simulated_ISR1_task \n");
_task_block();
}
/* Create the ISR task */
task_id_2 = _task_create(0, ISR_2_TASK, 0);
if (task_id_2 == MQX_NULL_TASK_ID)
{
printf("Could not create simulated_ISR2_task \n");
_task_block();
}
while (TRUE)
{
_time_delay(1000);
}
}
/* EOF */
解決済! 解決策の投稿を見る。
Hello amleng,
watchdog component can register only one function to the interrupt vector, the second time it fails because it was initialized already.
_lwsem_wait((LWSEM_STRUCT_PTR)(&kernel_data->COMPONENT_CREATE_LWSEM));
if (kernel_data->KERNEL_COMPONENTS[KERNEL_WATCHDOG] != NULL) {
_lwsem_post((LWSEM_STRUCT_PTR)(&kernel_data->COMPONENT_CREATE_LWSEM));
_KLOGX2(KLOG_watchdog_create_component, MQX_OK);
return(MQX_OK);
} /* Endif */
Regards,
MartinK
I know its not related to your problem but I'm curious why are you using fflush(stdio)?
Why flush?
What does it do?
Hi drummer,
fflush causes any buffered data in stream to be written to file. It returns 0 if it succeeded, otherwise EOF. You can check some reference webpages to find out more information.
Its fflush(stdout), it shall not be used with stdin because this behavior is undefined.
Regards,
MartinK
thanks for your response.
I have a task that looks after serial communications on one of three serial ports of the MCF52259.
Since the hardware interface is RS485 I control the direction through an I/O that is controlled by a timer.
All I have to do is turn on the I/O and timer isr turns it off. I used to wait until the timer was finished through 10 millisecond
time delays but thought that fflush would be faster since I don't need to time out anymore.
Like this...
ioctl(rsi_enable_fh, GPIO_IOCTL_WRITE_LOG1, NULL);
_time_delay(1);
rsi_timer = ((no_bytes + 1) * 44000/rsi_baud);
_io_write (rsi_fh, snd_buf,no_bytes );
fflush(rsi_fh);
// while(rsi_timer > 0)
// _time_delay(10);
I let it run all last night and came back with the task in a "task queue blocked" and it never came back.
I am still using MQX version 3.6.
I suspect it was stuck in the fflush but can't be certain.
i have also similar situation of "Task Queue Blocked". how did you solve it?
Hello amleng,
watchdog component can register only one function to the interrupt vector, the second time it fails because it was initialized already.
_lwsem_wait((LWSEM_STRUCT_PTR)(&kernel_data->COMPONENT_CREATE_LWSEM));
if (kernel_data->KERNEL_COMPONENTS[KERNEL_WATCHDOG] != NULL) {
_lwsem_post((LWSEM_STRUCT_PTR)(&kernel_data->COMPONENT_CREATE_LWSEM));
_KLOGX2(KLOG_watchdog_create_component, MQX_OK);
return(MQX_OK);
} /* Endif */
Regards,
MartinK
Hi Martin,
I was trying to do the same thing. In the MQX RTOS documentation you see the following:
The MQX watchdog component provides a software watchdog for each task. If a single
task starves or runs beyond certain timing constraints, the watchdog provides a way to
detect the problem. Initially, the task starts its watchdog with a specific time value, and if
the task fails to stop or restart the watchdog before that time expires, MQX calls a
processor-unique, application-supplied expiry function that can initiate error recovery.
Before a task can use the watchdog component, the application must explicitly create it
by calling _watchdog_create_component() with the interrupt vector of the periodic
timer device and a pointer to the function that MQX will call, if a watchdog expires.
The way it is written implies that you use the same interrupt vector each time (i.e. BSP_TIMER_INTERRUPT_VECTOR).
So just for clarification for each task I have will need a separate timer interrupt vector associated with it.
Is that correct?
Thanks,
Brent