Hello Evgeny,
MQX includes two USB stacks:
- MQX Host and Device USB stack version 4.2.0: Legacy USB stack with minor changes and bugfixes. Includes support for legacy platforms only (same processors previously supported in MQX RTOS 4.1.1.)
- New Host and Device USB stack version 2 (same as in KSDK 1.2.0): New USB stack is available for following platforms : FRDM-K64F, FRDM-K22F, TWR-K21F120M, TWRK22F120M,TWR-K64F120M, TWR-K65F180M, TWR-VF65GS10, SVF52
USB_v2 projects don't have any build files for cw10gcc as exist in all other projects (bsp, psp, mfs, rtcs, etc....).
Regarding the ColdFire v3, the following board support packages were removed from the new MQX releasee and will be supported only as a part of MQX 3.8.1
TWR-MCF51AG, TWR-MCF51CN, TWR-MCF51JE, TWR-MCF51MM, TWR-MCF51QM, DEMOEM, DEMOAC, EVB51JM128, M5208EVB, M52223EVB, M52233DEMO, M52235EVB, M52277EVB, M53015EVB, M5329EVB, M54455EVB and MPC8308RDB
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------