Hi i am using MK20DN512ZVll10 series controller on which i need to run MQX based application, using serial boot loader.
question is : Can we make use of twrk2072M related bsp and PSP, ofcourse with minor tweeks at appropriate locations ? or is there any sepeate bsp and psp that i need to use run appln on thiscontroller.
Thanks,
-J
Hi Janardhan:
Yes , you are right. You can start with TWR-K20D72M BSP, and that maybe require some changes to the BSP.
.Different peripherals and peripheral drivers
.Different pins for the peripherals and GPIO
.Different clock source, clock configuration, and clock frequencies
.Custom dirvers
.Different MCU derivatives
Please refer to the following documents for more details, it is under the MQX installation folder
Freescale_MQX_4_2\doc\mqx\MQX_BSP_Porting_Guide.pdf
Freescale_MQX_4_2\doc\mqx\MQX_BSP_Porting_Example_User_Guide.pdf
Have a great day,
Daniel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------