twrk20 for MK20DN512ZVLL10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

twrk20 for MK20DN512ZVLL10

484 Views
janardhannl
Contributor I

Hi i am using MK20DN512ZVll10 series controller on which i need to run MQX based application, using serial boot loader.

question is : Can we make use of twrk2072M related bsp and PSP, ofcourse with minor tweeks at appropriate locations ? or is there any sepeate bsp and psp that i need to use run appln on thiscontroller.

Thanks,

-J

0 Kudos
Reply
1 Reply

395 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Janardhan:

Yes , you are right.  You can start with TWR-K20D72M BSP, and that maybe require some changes to the BSP.

.Different peripherals and peripheral drivers

.Different pins for the peripherals and GPIO

.Different clock source, clock configuration, and clock frequencies

.Custom dirvers

.Different MCU derivatives

Please refer to the following documents for more details, it is under the MQX installation folder

Freescale_MQX_4_2\doc\mqx\MQX_BSP_Porting_Guide.pdf

Freescale_MQX_4_2\doc\mqx\MQX_BSP_Porting_Example_User_Guide.pdf

Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply