Hi,
I'm new here. Maybe someone can help me.
I have the TWR-K60 Board and downloaded the SDK with FreeRTOS support.
I selected the lwip_tcpecho_demo_freertos demo. But to my suprise I cannot compile it.
Everything is fresh installed. I'm confused as I don't believe that NXP would offer a demo to the whole community that doesn't work.
It seems it doesn't use the lower RAM. What is wrong here?
Memory region Used Size Region Size %age Used
PROGRAM_FLASH: 56216 B 512 KB 10.72%
SRAM_UPPER: 81988 B 64 KB 125.10%
SRAM_LOWER: 0 GB 64 KB 0.00%
c:/nxp/mcuxpressoide_11.1.1_3241/ide/plugins/com.nxp.mcuxpresso.tools.win32_11.1.0.202001081728/tools/bin/../lib/gcc/arm-none-eabi/8.3.1/../../../../arm-none-eabi/bin/ld.exe: twrk60d100m_demo_apps_lwip_lwip_tcpecho_freertos.axf section `.heap' will not fit in region `SRAM_UPPER'
c:/nxp/mcuxpressoide_11.1.1_3241/ide/plugins/com.nxp.mcuxpresso.tools.win32_11.1.0.202001081728/tools/bin/../lib/gcc/arm-none-eabi/8.3.1/../../../../arm-none-eabi/bin/ld.exe: region `SRAM_UPPER' overflowed by 16452 bytes
collect2.exe: error: ld returned 1 exit status
FLEX_RAM: 0 GB 4 KB 0.00%
make: *** [makefile:46: twrk60d100m_demo_apps_lwip_lwip_tcpecho_freertos.axf] Error 1
"make -r -j8 all" terminated with exit code 2. Build might be incomplete.
21:56:48 Build Failed. 3 errors, 0 warnings. (took 8s.253ms)
Greetings
mangkut
已解决! 转到解答。
Hi Marcus:
I would suggest you put the global data to SRAM_LOWER. Please refer to below picture.
Regards
Daniel
Ok, this works. Thanx Daniel.
Another thing... as I figured out that the most Kinetis EVAL-Boards are fitted with a KXXFN CPU there is no EEPROM via FlexRAM possible. As I understood only with FX CPUs.
I want port code from a Atmel CPU to an Kinetis. But I need to store user config data. The Atmel has EEPROM which I use for it. I don't want to build hardware for testing it.
Is it somehow possible to store user data without having this 4k FlexRAM?
My TWR-K60DN512 doesn't support EEPROM via FlexRAM if I understood right.
I used the SDK Builder on the Web-Site similar to the description in the followed link:
Generating a downloadable MCUXpresso SDK v.2 package
There you can select FreeRTOS
Than I downloaded it and simply drag and drop it to the project.
Then it offers you both, bm and FreeRTOS in the demo selections. But FreeRTOS doesn't work.
Regards
Marcus
Could you please let me know your SDK version and the IDE version?
Could you download the latest sdk from Welcome | MCUXpresso SDK Builder and try it again?
Regards
Daniel