_time_delay_internal remains in Time Delay Blocked State

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

_time_delay_internal remains in Time Delay Blocked State

1,227 Views
louiemoye
Contributor III

Any ideas why a call to _time_delay(100) would result in that task never returning from _time_delay_internal?  It looks like it hangs after the call to _sched_execute_scheduler_internal(); at the end of the _time_delay_internal function.  This is a task that executed correctly for a random number if iteration before being blocked.  I have a One Second Interrupt running at priority 8 - I tried changing to Priority 10 with no luck.  My tasks are all FIFO time-sliced at 50mS all at Priority 8.  Also, all the task stacks seem to be at reasonable usage levels.

I'm running on K70 using MQX 4.1, and CodeWarrior 10.6.

Thanks,

Louie 

0 Kudos
Reply
2 Replies

972 Views
soledad
NXP Employee
NXP Employee

Hi,

Could you please share your code in order to reproduce the issue.

Regards

Soledad

0 Kudos
Reply

972 Views
louiemoye
Contributor III

Soledad - this is the function that hangs.  It hangs in _time_delay_internal, which is called from the _time_delay(100) below.  Also following is the interrupt event that runs, which I suspect is playing a role in the lockup:  

void MotorDriver::SetDFROpto(bool bEnable)
{
if (bEnable)
{
GPIO_PTF_SetFieldBits(GPIO_PTF_DeviceData, DFR_OPTO_EN, 0x01);
_time_delay(100); 
}
else
GPIO_PTF_ClearFieldBits(GPIO_PTF_DeviceData, DFR_OPTO_EN, 0x01);
}

I also had this but removed the mutex to ensure I didn't have a deadlock issue

void MotorDriver::SetDFROpto(bool bEnable)
{
_mutex_lock(m_motorMutexDFR);
if (bEnable)
{
GPIO_PTF_SetFieldBits(GPIO_PTF_DeviceData, DFR_OPTO_EN, 0x01);
_time_delay(100);

}
else
GPIO_PTF_ClearFieldBits(GPIO_PTF_DeviceData, DFR_OPTO_EN, 0x01);
_mutex_unlock(m_motorMutexDFR);
}

//One second interrupt from the FPGA that states the detectors are ready to be read
void OneSec_OnInterrupt(LDD_TUserData *UserDataPtr)
{
void* td_ptr = _task_get_td(ARUBA::det_val_task_id); //MQX Ref Manual p373

if ((td_ptr != NULL))
{
_task_ready(td_ptr); //13 is the DetVal task
}
else
{
dprint("something horrible happened with unblocking the det val task");
}

// Run PIDS periodic task after Detector Value task, since it depends on the
// Detector Values.
// WARNING: Using _task_ready() causes infinite loops in the lwevent_wait() functions
InterruptEventManager::GetInstance()->ISR_EVTCallBackHandler(InterruptEventManager::PIDS_TASK_ENABLE);

}

0 Kudos
Reply